Other Parts Discussed in Thread: AM3358
Tool/software: Linux
Hi,
I have the GPMC configuration on a am3358 device:
-nandflash connect to CS0 of GPMC with async read/write, 8 bit device width.
-SRAM connect to CS1 of GPMC with non-multiplexed address/data bus, and sync read/write, 16 bit device width.
-use ti sdk 8.0, and kernel running from nandflash success.
When I access SRAM, low pulse can be detect at CS1 pin, but no signal can be detect at gpmc_clk pin and can't
get right data.
the following is my configuration in dts file:
&gpmc {
status = "okay";
pinctrl-names = "default", "sleep";
pinctrl-0 = <&nandflash_pins_default>;
pinctrl-1 = <&nandflash_pins_sleep>;
ranges = <0 0 0x08000000 0x10000000 /* CS0: NAND */
1 0 0x13000000 0x1000000 /* CS1: dual_business 16M*/
>;
nand@0,0 {
reg = <0 0 0>; /* CS0, offset 0 */
ti,nand-ecc-opt = "bch8";
ti,elm-id = <&elm>;
nand-bus-width = <8>;
gpmc,device-width = <1>;
gpmc,sync-clk-ps = <0>;
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <44>;
gpmc,cs-wr-off-ns = <44>;
gpmc,adv-on-ns = <6>;
gpmc,adv-rd-off-ns = <34>;
gpmc,adv-wr-off-ns = <44>;
gpmc,we-on-ns = <0>;
gpmc,we-off-ns = <40>;
gpmc,oe-on-ns = <0>;
gpmc,oe-off-ns = <54>;
gpmc,access-ns = <64>;
gpmc,rd-cycle-ns = <82>;
gpmc,wr-cycle-ns = <82>;
gpmc,wait-on-read = "true";
gpmc,wait-on-write = "true";
gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <0>;
gpmc,clk-activation-ns = <0>;
gpmc,wait-monitoring-ns = <0>;
gpmc,wr-access-ns = <40>;
gpmc,wr-data-mux-bus-ns = <0>;
/* MTD partition table */
/* All SPL-* partitions are sized to minimal length
* which can be independently programmable. For
* NAND flash this is equal to size of erase-block */
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "NAND.SPL";
reg = <0x00000000 0x000020000>;
};
partition@1 {
label = "NAND.SPL.backup1";
reg = <0x00020000 0x00020000>;
};
partition@2 {
label = "NAND.SPL.backup2";
reg = <0x00040000 0x00020000>;
};
partition@3 {
label = "NAND.SPL.backup3";
reg = <0x00060000 0x00020000>;
};
partition@4 {
label = "NAND.u-boot-spl-os";
reg = <0x00080000 0x00040000>;
};
partition@5 {
label = "NAND.u-boot";
reg = <0x000C0000 0x00100000>;
};
partition@6 {
label = "NAND.u-boot-env";
reg = <0x001C0000 0x00020000>;
};
partition@7 {
label = "NAND.u-boot-env.backup1";
reg = <0x001E0000 0x00020000>;
};
partition@8 {
label = "NAND.kernel";
reg = <0x00200000 0x00800000>;
};
partition@9 {
label = "NAND.rootfs";
reg = <0x00700000 0x0F900000>;
};
};
nor@1,0 {
compatible = "cfi-flash";
linux,mtd-name= "intel,pf48f6000m0y1be";
#address-cells = <1>;
#size-cells = <1>;
reg = <1 0 0x1000000>; /* CS1, offset 0 */
bank-width = <2>;
gpmc,sync-read;
gpmc,sync-write;
gpmc,wait-pin = <0>;
gpmc,wait-on-read;
gpmc,wait-on-write;
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <186>;
gpmc,cs-wr-off-ns = <186>;
gpmc,adv-on-ns = <12>;
gpmc,adv-rd-off-ns = <48>;
gpmc,adv-wr-off-ns = <48>;
gpmc,oe-on-ns = <54>;
gpmc,oe-off-ns = <168>;
gpmc,we-on-ns = <54>;
gpmc,we-off-ns = <168>;
gpmc,rd-cycle-ns = <186>;
gpmc,wr-cycle-ns = <186>;
gpmc,access-ns = <114>;
gpmc,page-burst-access-ns = <6>;
gpmc,bus-turnaround-ns = <12>;
gpmc,cycle2cycle-delay-ns = <18>;
gpmc,wr-data-mux-bus-ns = <90>;
gpmc,wr-access-ns = <186>;
gpmc,cycle2cycle-samecsen;
gpmc,cycle2cycle-diffcsen;
partition@0 {
label = "dual-nor";
reg = <0 0x1000000>;
};
};
What's wrong with my configuration?
Best Regards!