Tool/software: Linux
Hi,
TI,
What the sdk03.02 of am5728 can not install in the 64bits ubuntu?I download the sdk at the 2017/1/4.Now that,the download link of am5728 sdk is close by TI.Why?
BR,
vefone
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vefone,
vefone said:What the sdk03.02 of am5728 can not install in the 64bits ubuntu?
SDK03.02 can be installed on Ubuntu 64-bit OS. I am having Ubuntu12.04 64-bit, and I can install successful.
pbotev@mms-0306:~/workdir/AM57x$ ls -al ti-processor-sdk-linux-am57xx-evm-03.02.00.05-Linux-x86-Install.bin
-rwxr-xr-x 1 pbotev mmsol 2113549568 Jan 23 10:49 ti-processor-sdk-linux-am57xx-evm-03.02.00.05-Linux-x86-Install.bin
pbotev@mms-0306:~/workdir/AM57x$ uname -a
Linux mms-0306 3.13.0-77-generic #121~precise1-Ubuntu SMP Wed Jan 20 18:02:20 UTC 2016 x86_64 x86_64 x86_64 GNU/Linux
pbotev@mms-0306:~/workdir/AM57x$ ls ti-processor-sdk-linux-am57xx-evm-03.02.00.05
bin board-support docs example-applications filesystem linux-devkit Makefile Rules.make setup.sh
Can you provide the output you have on your side of the above commands?
I will check this with the team and come back to you.
Regards,
Pavel