This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3358: External parallel memory interface

Part Number: AM3358

Tool/software: Linux

Hi ,

We need to interface a 8 bit parallel memory device (FPGA ) to  AM3358 processor .

The FPGA Device has got 8 parallel data lines and 3 address lines.

Please suggest me which interface to go with . EMIF or GPMC ?

What will be the max speed if i go with GPMC ?

Also please tell me how GPMC is mapped with DMA ?

Is it possible for me to validate the FPGA device using Beagle Bone Black Board with above mentioned requirements.?

Thanks,

Chandan