This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4379: 180 degrees display rotation

Part Number: AM4379

Tool/software: Linux

Hi All

Customer is asking how they can rotate their display as mechanically they displays re rotated 180 degrees

that based on the way our lcd panels are being installed, we are going to need to rotate the display 180°.  Is there hardware support for this in the AM437x?  Searching around I found a few suggestions like running echo 2 > /sys/class/graphics/fb0/rotate that didn't work for me, but no definitive answer on whether this was supported.

We are building a kernel based off of the 02.00.00 release and are using build-root based off of the
2015.08 release to build our userspace.

(the kernel from the 02.00.00 TI SDK release)

 

Thanks

Jeff Coletti