This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Processor suggestion for H.264 video decoding

Hi all,

I want to design a board with the following inputs and outputs:

Input:

  • USB port (to read 1920x1080 h.264 mp4 video files from flash memory)
  • microSD card (to boot OS, like linux, or Android)
  • LAN (to connect to internet)

Output:

  • 24-bit RGB data (to give to an LVDS Serializer/Transmitter IC which connects to 40 inch LCD panels)

I know that AM57xx family is capable of doing this, but they are not cheap!

Would you suggest a cheaper solution?