This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Jacinto 6 platform: latest schematics reference for suspend-to-RAM (ideally for J6RSP)

Hello,

can you point me to the latest schematics reference for suspend-to-RAM (ideally for J6RSP)?

Thanks, Stefan

  • Hi Stefan,

    I have forwarded your question to an expert.

    Regards,
    Yordan
  • The J6Entry EVM does include the hardware configuration/options to support the different levels of suspend-2-ram.

    Level 1: DDR memory content preserved across a warm reset.
    - From hardware perspective, this mode requires a pull-down on CKE

    Level 2: DDR memory content preserved across a cold reset.
    - From hardware perspective, this mode requires Level 1 (PD on CKE) plus it requires external control of DDR Reset

    Level 3: DDR memory content preserved across a power cycle
    - From hardware perspective, this mode requires Level 1 and Level 2 (PD on CKE, external DDR Reset control) and separate power control for DDR/VREF

    There are silicon errata which might affect recovering from self refresh mode, and I currently in discussions to determine if/how they affect these different levels. I will update the thread when I have more clear understanding.

    Thanks.
    Robert
  • Hi,

    There was a suggested answer and since there has been no activity on this thread for more than a week,
    the suggested answer was marked as verify. Please feel free to select the "Reject Answer" button and reply with more details.

    Regards,
    Yordan
  • Yes - I did confirm the silicon errata is specific to warm reset conditions only, and does not affect cold/power on reset conditions - and therefore does not impact suspend to ram operation.
    Thanks
    Robert
  • Hello,

    can you please add which J6RSP rails are kept active (if at all) for suspend to RAM? and if there is any rail, what is the current consumption?

    Thanks, Stefan

  • It depends on which level of Suspend To RAM you are referring.  For levels I and II - all power rails remain active.  For Level 3, only DDR power rails remain active (No SoC power rails are powered).  In all 3 levels - the DDR memory device is place into self refresh mode.  The memory data sheet should specify the power requirements for self refresh mode.