Part Number: TMS320C5517
Tool/software: Code Composer Studio
Hello, everyone.
I have read "Using the TMS320C5517 Bootloader.pdf", but I still don't know how to burn exactly.
It says:
Once a boot image (*.bin) is generated, you can burn the boot image into the supported peripherals using
a utility called programmer, which is part of the TMS320C55x Chip Support Libraries (CSL) (see
www.ti.com/.../sprc133). The utility runs on each device using an emulator with Code Composer
Studio.
But How do I use csl to burn the program? Csl is a collection of functions. How to use it? Do I need to write a additional program using csl functions to burn the application code into external FLASH?
If so, how to write the program? I didn't see any example....
I want to burn it to GD25Q80C(a serial flash) using SPI interface.
thanks