Part Number: TMS320DM365
Hi,
DM36x supports 4x4 or 5x3 keyscan. My customer only needs 3x3 key board and he wants to know if he can configure two keyscan pins (keyA3/keyB3) to GPIO and if this will effect the keyscan function.
I think there is no problem for GPIO operation after pinmux setting. But I am not sure when the keyscan pins are configured as GPIO, what's the status of the path which connected to these two keyscan pin in internal keyscan module. Will it keep a fix status or it will change by the real pins?
Would you pls help to check when keyA3/keyB3 pins are configured as GPIO, will it effect the keyscan function when they toggle high or low?