Part Number: AM3358
There are 16 pins that are used to select booting sequence of AM3358 (R1~R4, T1~T4, U1~U4, V2~V5). I am using 100K resistors to pull the pins to high or low. Since the booting sequence is fixed in my design, can I just use straight connection to 3.3V or GND instead of using resistors to configure booting sequence?
Thank you.