hi,
I would like to connect a NOR flash to the OMAP3530 GPMC.
The OMAP only supports a 2KB NOR, but the AM3715/03 GPMC subsystem wiki show that if you use an external latch, you can connect any 16-NOR.
here is the link: http://processors.wiki.ti.com/index.php/AM3715/03_GPMC_Subsystem#16-bit_NOR_with_external_latch.C2.A0
The question is if I can connect a NOR flash in the same way to the OMAP.
Thanks,
Jose