Part Number: AM3352
Tool/software: Linux
Hi
I have taken over a project that is using a board based closely on the beaglebone black.
I am in the process of trying to bring this project up to date with the most recent TI-SDK
(which uses linux-4.4.19+gitAUTOINC+db0b54cdad-gdb0b54cdad/ and u-boot-2016.05+gitAUTOINC+2f757e5b2c-g2f757e5b2c/ )
At present it has an old U-boot that succeeds sufficiently to enable me to load a kernel and DTB via NFS. The output of the old U-Boot looks as though it has a few issues; but manages to get through to a command line. From here I am trying to load a new U-boot via TFTP
This looks to launch then almost immediately crash:
U-Boot# setenv autoload no; dhcp; setenv serverip 10.255.0.148; tftp 0x80800000 u-boot.bin; go 0x80800000
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
DHCP client bound to address 10.255.3.255
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 10.255.0.148; our IP address is 10.255.3.255
Filename 'u-boot.bin'.
Load address: 0x80800000
Loading: ############################
1.7 MiB/s
done
Bytes transferred = 397594 (6111a hex)
## Starting application at 0x80800000 ...
U-Boot 2016.05-00119-gb5d9570-dirty (Feb 27 2017 - 16:08:43 +1100)
Watchdog enabled
I2C: ready
DRAM: 512 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - MMC init failed, using default environment
Could not get board ID.
<ethaddr> not set. Validating first E-fuse MAC
Net: data abort
pc : [<9ff851c8>] lr : [<9ff526eb>]
reloc pc : [<808331c8>] lr : [<808006eb>]
sp : 9ef29428 ip : 00000061 fp : 00000017
r10: 8084eae8 r9 : 9ef31ed8 r8 : 9ffeca58
r7 : 9ff9efc0 r6 : 9ef31fb0 r5 : 44e10600 r4 : 9ff9d050
r3 : 4030b847 r2 : 9ff8dbb6 r1 : 9ff8dbb0 r0 : ffffffff
Flags: Nzcv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
resetting ...
This smells to me like there is either something defined in my DTS that should not be (or conversely that there is something fundamental missing).
Is anyone able to shed any light on how I might use the debug that has been output to track down where the culprit is hiding?
Thanks for any help.
Best regards,
Richard
for interet the output from the older U-Boot looks like:
U-Boot SPLLL 2014.07-00107-gd28f2b9-dirty (Nov 22 2016 - 11:44:08) Could not probe the EEPROM; something fundamentally wrong on the I2C bus. Could not get board ID. ddr params. Could not probe the EEPROM; something fundamentally wrong on the I2C bus. Could not get board ID. Setting pinmux bbb lt fake mux done Could not probe the EEPROM; something fundamentally wrong on the I2C bus. Could not get board ID. SDRAM init ddr init fake start ddr init fake end board init malloc timer Could not probe the EEPROM; something fundamentally wrong on the I2C bus. Could not get board ID. board init 600 board not bone PIMC success tps 0 tps 1 tps 2 tps 3 tps 4 tps 5 osc success board init end boot device boot debug device U-boot load start U-boot load end %d U-Boot 2014.07-00107-gd28f2b9-dirty (Nov 22 2016 - 12:36:41) I2C: readyEZ DRAM: DRAM config 512 MiB init trace start serial MMCEZ: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Using default environment Could not probe the EEPROM; something fundamentally wrong on the I2C bus. Could not get board ID. late init. Net: <ethaddr> not set. Validating first E-fuse MAC Could not probe the EEPROM; something fundamentally wrong on the I2C bus. Could not get board ID. late init. Enable rmii Existing Phy not found phy id 508209 0 -1 cpsw New Phy 0 found usb eth init. usb eth init end. cpsw, usb_ether Hit any key to stop autoboot: 0 U-Boot# <INTERRUPT> U-Boot#