Other Parts Discussed in Thread: OMAP3530
Hi,
I have been searching around for an answer to whether it is possible to boot from a USB stick in the same way as booting from an SD card. I understand there is a tool, which in conjunction with U-boot V2, allows you to boot the OMAP3530 over USB when connected to a host machine. However, my aim is to boot the OMAP3530 using only a USB stick without the need for a connection to a host machine (USB, Ethernet, Serial).
Is is possible to configure the OMAP3530 to recognise a bootloader on the USB stick in the same way it can recognise the MLO file on a SD card? I currently have a Beagleboard Rev C4 and an OMAP3530 EVM for development.
Any help on this will be great.
Andy