This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: RX check-box in Pinmux Tool

Guru 10235 points

Part Number: AM3352

Hello, TI Experts,

 

We have a question about "RX-check-box" of PINMUX-TOOL for AM335x.

We found related E2E thread as below.

http://e2e.ti.com/support/arm/sitara_arm/f/791/t/515012

http://e2e.ti.com/support/arm/sitara_arm/f/791/t/383189

 

From this E2E thread, our understanding is as follows;

  - The RXACTIVE bit is just an enable pin to the input buffer.(It is NOT for direction control.)

    - Rx-check-box is the Input Enable value for the PAD (RXACTIVE bit).

    - For INPUT-pin, the input buffer should be enabled by checking Rx-check-box.

    - For INOUT-pin, the input buffer should be enabled by checking Rx-check-box.

    - For OUTPUT-pin, enabling the input buffer is not mandatory,

      unless specific instructions  are given from  the datasheet  or guidelines like below.

           http://processors.wiki.ti.com/index.php/AM335x_Schematic_Checklist#MMC

         - Even if Rx-check-box is checked, the output pin function works properly.

         - Rx-check-box is recommended to be un-checked for leakage point of view in general.

 

Is this understanding correct?

 

Best regards