Tool/software: Linux
Hi,
refer to: http://www.ti.com/lit/ds/symlink/tci6636k2h.pdf
- Table 6-24 list the ARM CorePac interrupt inputs
It is mentioned that "Event No. 0 is identical to ARM GIC interrupt ID 0."
But e.g. the PCIE_INT1 which has interrupt ID 27, is in reality the Virtual Timer based on the GIC 400 spec.
http://infocenter.arm.com/help/topic/com.arm.doc.ddi0471b/DDI0471B_gic400_r0p1_trm.pdf
How to translate the interrupt ID mapping in the HW manual to the GIC?
btw. I also didn't found this information on
processors.wiki.ti.com/.../Configuring_Interrupts_on_Keystone_Devices
Thanks!
- Wladislav Wiebe