Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

De-interlace based on DM6467

Other Parts Discussed in Thread: TVP5146

Hi all, I am now capturing video through TVP5146 based on DM6467. Here I get a problem. The video source is interlaced, so when I try to display progressive video, there are obvious tailings for moving pictures. I think maybe I should add de-interlace process to eliminate this problem. But I don't know how to do it, can this be carried out making use of the hardware of DM6467 such as resizer? Anyone who can give me some suggestions?

  • vivian Wang said:
    But I don't know how to do it, can this be carried out making use of the hardware of DM6467 such as resizer? Anyone who can give me some suggestions?

    A simple weave deinterlacing could be done by the DMA which is probably what you are seeing now, however to have a good deinterlace you would really need a motion adaptive deinterlacing algorithm which would not be done on the resizer, but more likely with the DSP. If you wanted to do a line doubling deinterlace method you could use the resizer to scale up one field to the size of the full frame (as discussed in this application note), though this would lose half of your vertical resolution it would remove the 'mouse teeth' artifacts on fast moving objects. Some various deinterlacing techniques are described on the deinterlacing wikipedia article, this should give you an idea of some of the available options, though I do not know of any third party motion adaptive deinterlacers available for DM6467.

    EDIT: Note the DM6467 has a different video pipeline from the DM6446 used in the above mentioned application note, it has a VDCE, so the concept is the same but the register level implementation is different.

  • The DM6467 Video Data Conversion Engine (VDCE) supports the following features:

    Resize function on horizontal (HRSZ) and vertical (VRSZ) with ratio defined by 256/N (N is a natural
    number that ranges from 256 to 2048) with 4 taps interpolation,

    This means that can not be realized image to enlarge, can not  do a line doubling deinterlace  yet!

    Why h264enc/h264fhdvenc support deinterlace function by Motion Compensation?

     

     

     

  • How did you learn h264enc/h264fhdvenc support deinterlace function by Motion Compensation as the VDCE doesn't support the enlarge of picutures? 

  • So Sorry! What I really want to say is that:
    why doesn't h264enc/h264fhdvenc support deinterlace function by Motion Compensation?

  • WE do not  have HW support for De-interlacing on DM6467. One way to do the de-interlacing would be to use the DSP/C64x+ . A simple De-interlacing technique of averaging the pixels should not consume much cycles on the DSP

    Regards,

    Kapil

  • Hi, Kapli,

     

    I really doubt about "A simple De-interlacing technique of averaging the pixels should not consume much cycles on the DSP", actually, if you run the video_loopback_copy dmai demo, even with D1 video, you will be taken about 50% percent of CPU.... I do believe the only way to do so is give the simplest job to DSP........ Too BAD.