Part Number: OMAPL138B-EP
Other Parts Discussed in Thread: OMAPL138
Tool/software: TI-RTOS
I have buit application based on SYS/BIOS from generated code from simulink model by CCSv5 and i encounter error show below:
Description Resource Path Location Type
#10010 errors encountered during linking; "audio_delay.out" not built audio_delay C/C++ Problem
#10264 DDR2 memory range overlaps existing OMAPL138.cmd /audio_delay line 41 C/C++ Problem
#10264 SHDSPL1DRAM memory range overlaps OMAPL138.cmd /audio_delay line 34 C/C++ Problem
#10264 SHDSPL1PRAM memory range overlaps OMAPL138.cmd /audio_delay line 33 C/C++ Problem
#10264 SHDSPL2RAM memory range overlaps OMAPL138.cmd /audio_delay line 32 C/C++ Problem
#10264 SHRAM memory range overlaps existing OMAPL138.cmd /audio_delay line 40 C/C++ Problem
<a href="file:/F:/Programs/ccsv6/ccsv6/tools/compiler/dmed/HTML/10234.html">#10234-D</a> unresolved symbols remain audio_delay C/C++ Problem
unresolved symbol _Aic31_init, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
unresolved symbol _Aic31_IOMFXNS, first referenced in ./audio_delaycfg.obj audio_delay C/C++ Problem
unresolved symbol _Aic31_PARAMS, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
unresolved symbol _Audio_init, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
unresolved symbol _Audio_IOMFXNS, first referenced in ./audio_delaycfg.obj audio_delay C/C++ Problem
unresolved symbol _Audio_PARAMS, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
unresolved symbol _edma3init, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
unresolved symbol _hEdma, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
unresolved symbol _I2c_init, first referenced in ./c6748evm_i2c.obj audio_delay C/C++ Problem
unresolved symbol _I2c_IOMFXNS, first referenced in ./audio_delaycfg.obj audio_delay C/C++ Problem
unresolved symbol _I2c_PARAMS, first referenced in ./c6748evm_i2c.obj audio_delay C/C++ Problem
unresolved symbol _Mcasp_init, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
unresolved symbol _Mcasp_IOMFXNS, first referenced in ./audio_delaycfg.obj audio_delay C/C++ Problem
unresolved symbol _Mcasp_PARAMS, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
unresolved symbol _Psc_ModuleClkCtrl, first referenced in ./c6748evm_aic31.obj audio_delay C/C++ Problem
I use default cmd OMAPL138.cmd show below:
MEMORY
{
#ifdef DSP_CORE /* DSP exclusive memory regions */
DSPL2ROM o = 0x00700000 l = 0x00100000 /* 1MB L2 DSP local ROM */
DSPL2RAM o = 0x00800000 l = 0x00040000 /* 256kB L2 DSP local RAM */
DSPL1PRAM o = 0x00E00000 l = 0x00008000 /* 32kB L1 DSP local Program RAM */
DSPL1DRAM o = 0x00F00000 l = 0x00008000 /* 32kB L1 DSP local Data RAM */
#endif
SHDSPL2ROM o = 0x11700000 l = 0x00100000 /* 1MB L2 Shared Internal ROM */
SHDSPL2RAM o = 0x11800000 l = 0x00040000 /* 256kB L2 Shared Internal RAM */
SHDSPL1PRAM o = 0x11E00000 l = 0x00008000 /* 32kB L1 Shared Internal Program RAM */
SHDSPL1DRAM o = 0x11F00000 l = 0x00008000 /* 32kB L1 Shared Internal Data RAM */
EMIFACS0 o = 0x40000000 l = 0x20000000 /* 512MB SDRAM Data (CS0) */
EMIFACS2 o = 0x60000000 l = 0x02000000 /* 32MB Async Data (CS2) */
EMIFACS3 o = 0x62000000 l = 0x02000000 /* 32MB Async Data (CS3) */
EMIFACS4 o = 0x64000000 l = 0x02000000 /* 32MB Async Data (CS4) */
EMIFACS5 o = 0x66000000 l = 0x02000000 /* 32MB Async Data (CS5) */
SHRAM o = 0x80000000 l = 0x00020000 /* 128kB Shared RAM */
DDR2 o = 0xC0000000 l = 0x20000000 /* 512MB DDR2 Data */
#ifndef DSP_CORE /* ARM exclusive memory regions */
ARMROM o = 0xFFFD0000 l = 0x00010000 /* 64kB ARM local ROM */
ARMRAM o = 0xFFFF0000 l = 0x00002000 /* 8kB ARM local RAM */
#endif
}
SECTIONS
{
.text > SHRAM
.stack > SHRAM
.bss > SHRAM
.cio > SHRAM
.const > SHRAM
.data > SHRAM
.switch > SHRAM
.sysmem > SHRAM
.far > SHRAM
.args > SHRAM
.ppinfo > SHRAM
.ppdata > SHRAM
/* TI-ABI or COFF sections */
.pinit > SHRAM
.cinit > SHRAM
/* EABI sections */
.binit > SHRAM
.init_array > SHRAM
.neardata > SHRAM
.fardata > SHRAM
.rodata > SHRAM
.c6xabi.exidx > SHRAM
.c6xabi.extab > SHRAM
}
I use:
- CCS v5.2.1
- SYS/BIOS 5_41_11_38
I don't know cause of problem, can't you help me solve this.
Thanks in advanced!