Part Number: AM3352
Other Parts Discussed in Thread: TPS650250
Hi,
We have a new project on AM3352 (1GHz) and we need advice in selecting right PMIC.
As the input voltage is 3.6V to 6.0V, only PMIC option we have is TPS650250..
But the power solution in the wiki page mentions TPS650250 supports only OPP50/OPP100.
Is there any reason why TPS650250 cannot be used for Turbo and Nitro?
processors.wiki.ti.com/.../AM335x_Hardware_Design_Guide
As per the AM335x datasheet current consumption for Nitro is 1000mA (MAX).
Whereas TPS650250's DCDC1 can supply upto 1600mA(MAX).
And this application even though runs at 1GHz it uses only minimal peripherals,
so we wonder if we could use TPS650250 for Turbo and Nitro?
Best Regards
Kummi