Part Number: TMS320DM355
Other Parts Discussed in Thread: TVP5146
Tool/software: Linux
Its seems that using SPI Bus 1 and EDMA is not possible.
Spi 1 wont work unless the following Section in the dm355,c file is commented out. which ALSO causes video encoding to Fail. This make EVEN having a SPI1 useless if you are going to use the processor to capture / encode video. what sense does that make?
Encode demo started.
tvp514x 1-005d: tvp514x_s_routing:
tvp514x 1-005d: tvp5146 (Version - 0x03) found at 0xba (DaVinci I2C adapter) (Expro)
tvp514x 1-005d: tvp514x_s_routing: 6
tvp514x 1-005d: tvp514x_querystd:
tvp514x 1-005d: tvp514x_querystd: 6
tvp514x 1-005d: tvp514x_s_routing:
EDMAK Error: dma_ioctl: REQUESTDMA failed: -16
EDMA Error: EDMA_IOCREQUESTDMA error
Error: Failed to create video encoder: mpeg4enc
Commented Lines.... out of DM355.c
static struct resource edma_resources[] = {
{
.name = "edma_cc0",
.start = 0x01c00000,
.end = 0x01c00000 + SZ_64K - 1,
.flags = IORESOURCE_MEM,
},
{
.name = "edma_tc0",
.start = 0x01c10000,
.end = 0x01c10000 + SZ_1K - 1,
.flags = IORESOURCE_MEM,
},
{
.name = "edma_tc1",
.start = 0x01c10400,
.end = 0x01c10400 + SZ_1K - 1,
.flags = IORESOURCE_MEM,
},
{
.name = "edma0",
.start = IRQ_CCINT0,
.flags = IORESOURCE_IRQ,
},
// DAS - Removed for SPI 1?
/*
{
.name = "edma0_err",
.start = IRQ_CCERRINT,
.flags = IORESOURCE_IRQ,
},
*/
/* not using (or muxing) TC*_ERR */
};