Hello,
One of my customers is using the AM4377BZDND80. All their voltages (VDDS, VDDS_CLKOUT VDDSHVx, etc.) are 1.8V. the power up sequence is acording to the below plot:
The requirements of the power down sequence are mentioned in the datasheet, but they are not clear to my customer.
1. The only specification here is about the below voltages: VDDS, VDDS_CLKOUT VDDSHVx – but since they are 1.8V, the customer believe that with them it won’t be a problem.
2. For the 1.2V and 1.1V - it is written that “The preferred way to sequence power down is to have all the power supplies ramped down sequentially in the exact reverse order of the power-up sequencing” – Is it mandatory to have the sequence on this order? What are the other options?
3. Additional input that they would like to get clarification is “All other external clocks to the device should be shut off” – can you explain?
4. This is their voltages plot: is the power sequencing here right? Is there a risk to damage the processor in this way?
Regards,
Meir.