Other Parts Discussed in Thread: SYSBIOS
I am using the network package ndk_evm6748_elf_helloWorld,
The version of NDK: 2.25.1.11 and NSP: 1.10.3.15
SYSBIOS 6.46.4.53.
I took the code of the example TCP echo server from the document SPRU524J–May 2001 p.104 and modified as following:
#include <netmain.h>
#include "helloWorld.h"
#include <ti/sysbios/knl/Task.h>
//
// dtask_tcp_hello() - UDP Echo Server Daemon Function
// (SOCK_DGRAM, port 7)
//
// Returns "1" if socket 's' is still open, and "0" if its been closed
//
int dtask_tcp_echo( SOCKET s, UINT32 unused )
{
struct timeval to;
int I;
char *pBuf;
int i,j;
HANDLE hBuffer;
(void)unused;
// Configure our socket timeout to be 5 seconds
to.tv_sec = NULL;//5;
to.tv_usec = 0;
setsockopt( s, SOL_SOCKET, SO_SNDTIMEO, &to, sizeof(to) );
setsockopt( s, SOL_SOCKET, SO_RCVTIMEO, &to, sizeof(to) );
I = 1;
setsockopt( s, IPPROTO_TCP, TCP_NOOPT, &I, 4 );
for(;;)
{
I = (int)recvnc( s, (void **)&pBuf, 0, &hBuffer );
// If we read data, echo it back
if(I > 0)
{
j=0;
for(i=0;i<200;i++)
{
if(send( s, stringData+j, 1000, 0) < 0)
{
break;
}
j=j+1000;
recvncfree( hBuffer );
}
}
// If the connection got an error or disconnect, close
else
break;
}
fdClose( s );
// Return "0" since we closed the socket
return(0);
}
=========================================================================================
stringData[] is a char array have a size of 20000. I am expecting those 200000 bytes char will be sent out. However, I only got about 100000 bytes. I tried to suspend running in debug mode. It looks like the program goes to the Idle_run() before the for loop is done. Tried to set break point at "break" right after send(), never reached.Can you give me some suggestions?
Thanks,
Andy