Tool/software: Linux
Hi all,
I want to do changes in v4l2 plugin. For that, i have successfully cross compiled gst-plugin-good-1.2.3 with am5728.
while running v4l2src pipeline gives error like below.
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
0:00:00.229419830 3984 0x129690 WARN v4l2 gstv4l2bufferpool.c:714:gst_v4l2_buffer_pool_qbuf:<v4l2bufferpool0> could not queue a buffer 0
0:00:00.229677496 3984 0x129690 WARN v4l2 gstv4l2bufferpool.c:714:gst_v4l2_buffer_pool_qbuf:<v4l2bufferpool0> could not queue a buffer 1
0:00:00.229813324 3984 0x129690 WARN v4l2 gstv4l2bufferpool.c:714:gst_v4l2_buffer_pool_qbuf:<v4l2bufferpool0> could not queue a buffer 2
0:00:00.229966721 3984 0x129690 WARN v4l2 gstv4l2bufferpool.c:714:gst_v4l2_buffer_pool_qbuf:<v4l2bufferpool0> could not queue a buffer 3
0:00:00.230091650 3984 0x129690 WARN v4l2 gstv4l2bufferpool.c:714:gst_v4l2_buffer_pool_qbuf:<v4l2bufferpool0> could not queue a buffer 4
0:00:00.230216091 3984 0x129690 WARN v4l2 gstv4l2bufferpool.c:714:gst_v4l2_buffer_pool_qbuf:<v4l2bufferpool0> could not queue a buffer 5
0:00:00.230337930 3984 0x129690 WARN v4l2 gstv4l2bufferpool.c:714:gst_v4l2_buffer_pool_qbuf:<v4l2bufferpool0> could not queue a buffer 6
0:00:00.230459931 3984 0x129690 WARN v4l2 gstv4l2bufferpool.c:714:gst_v4l2_buffer_pool_qbuf:<v4l2bufferpool0> could not queue a buffer 7
Any solution for this problem?
Regards,
Prerak