Hello everyone
I have designed a TMS320DM648 based board.Now I want to boot from network,but I can't receive the BOOTP request packet through the boot port.
The REFCLKP/N is 62.5 MHz on my board,and it works ok when I run an HelloWord ethernet program.The spraaj1c document says"Ethernet boot, I2C boot, and I2C boot modes are supported with ROM version 3.70." How can I confirm my dm648 chip 's ROM version?
Thanks in advance for all your help.