Other Parts Discussed in Thread: AM3358
Tool/software: TI-RTOS
Hello everyone,
at the moment I'm tring to evaluate if we could use the AM3358 to replace Cortex M3 microcontrollers in some applications.
As an evaluation-board i bought the BeagleBordBlack and installed code composer studio and the Ti-RTOS SDK. Now i'm really having a hard time to get so test code into the controller (i'm really more the hardware guy).
At first I treid to figuere out if it is possible to get the code directly to the Board (but without an external debugger - i don't have one here) this doesn't work right?
Then i tried to load the code to an SD card, but i dont quite understand how to do that. After i build my code i get an .out-file which has to be conveted in some way besfore i can load it on the CD card .But i dind't find anything newbe-friedly on how to do that. Can you help me with this?
Thanks in advance,
Christian