Part Number: TM4C129XNCZAD
Tool/software: TI-RTOS
Hello,
I'm using
- CCS Version: 6.1.0.00104,
- TIRTOS: tirtos_tivac_2_16_01_14,
- xdctools_3_32_01_22_core
i have many tasks in my projects, and i'm following uni-casting technique to forward some IP packets over UDP socket, but if i send some packets to multiple targets successively, i will get error (55 = No buffer space available) after the 7th target which indicates that there is no available buffer and because i'm limited in my buffer size so i added a delay between transmissions to the targets up to 100 milliseconds which should be significant but it didn't help and i'm still getting the same error.
my question is:
- did i miss something with the other tasks priorities compared to the NDK tasks that cause the IP packets to be delayed that much such that 100ms is n't that enough?
- for confirmation how the NDK buffer can be increased to reduce the effect of error (55)?
Thanks,
Mohammed Fawzy