Part Number: TDA3
Hello,
TDA3x has clkout[2:1] which can be used as a system clock for other devices.
A customer would like to use the clkout pin to be fed to DS90UB964:REFCLK input which is required jitter 100 ppm as shown below DM of UB964.
Can clkout pins of TDA3x be applied to DS90UB964:REFCLK?
Regards,
Yoshi Takano