I am considering TMS320DM368 for my H264 network streaming applicaition. My input video is 25 fps PAL at D1 resolution, same as my output video. It will be converted to digital, coded to H264, streamed over IP/ethernet, decoded and displayed. A pretty standard application. My main concern is encoding/decoding latency. So, if I connected two eval boards directly with an ethernet cable and use one as an encoder and one as a decoder, and with proper encoder/decoder/buffering...etc settings
1. What should be the minimum latency? Could it be well under 100 milliseconds?
2. What would be the key frame intervals (in frames) on the encoder side?
3. What would be the buffer in frames on the decoder side?
4. Would you recommend a different processor?
5. Can I add OSD symbols and text to the video with software on either side?