Part Number: AM4376
Questions from customer:
They would like to us the PRUs – ICSS0 (PRU0 and PRU1) for the Industrial Ethernet based fieldbus communications – PROFINET /EtherCAT (see picture).
-
Are two separate MAC addresses available for the two ETH0 and ETH1 RJ45 connectors?
-
Is it possible to assign 1 IP address to both ports or do each have to have 1 IP address each?
-
For the non-real time communication, they also need two separate Ethernet ports (ETH3 and ETH4)
-
Do both the ports have the same MAC and IP addresses (which would be “pre-provided” by TI)?
-
Could one of the ports (e.g. ETH4) be prioritized, and how is the communicated controlled by the Sitara – ARP tables? Routing tables?
-
Complementing the ICSS/PRU use, they would like to use the 2nd ICSS (ICSS1) for an EnDat 2.2 interface. Would that be possible?