Hi All,
We are doing a project of which Davinci DM6446 is used. We found that SPI device is not supported in DM6446 kernal(MontaVista 5.0 Linux-2.6.18).
In Kconfig file, it reads: SPI is only officially supported for DM646x and DM355.
So can anyone tell us how to modify the core or which pitch could be used to drive the SPI on DM6446? Many thanks!
regards,
swinter.