Part Number: EVMK2H
Other Parts Discussed in Thread: SYSBIOS, CCSTUDIO
Tool/software: TI-RTOS
Hi.
I set my PC these TI tools, Code Composer Studio V7 and Processor SDK 4.0.4 for EVMK2H.
I try to build example project presented TI. build is pretty good. but It has an error "Invalid SOC"
I check binaries, I find out new bin file, build is success I think.
Why the Error occurred?? and can I fix it? I attached console log file.
Regards.
Shin.
**** Build of configuration Debug for project PCIE_K2H_wSoCFile_C66BiosExampleProject ****
"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 8 all -O
gmake[1]: Entering directory 'C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject/Debug'
'Building file: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/k2h/c66/bios/pcie_sample_wSoCFile.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_32_01_22_core/xs" --xdcpath="C:/ti/edma3_lld_2_12_02_26/packages;C:/ti/ipc_3_44_00_00/packages;C:/ti/bios_6_46_01_38/packages;C:/ti/pdk_k2hk_4_0_4/packages;C:/ti/ndk_2_25_00_09/packages;C:/ti/uia_2_00_06_52/packages;C:/ti/ccsv7/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p ti.platforms.evmTCI6636K2H -r debug -c "C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3" "C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/k2h/c66/bios/pcie_sample_wSoCFile.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring pcie_sample_wSoCFile.xe66 from package/cfg/pcie_sample_wSoCFile_pe66.cfg ...
generating custom ti.sysbios library makefile ...
Inside EDMA3 Drv Sample getLibs
will link with ti.sdo.edma3.drv.sample:lib/tci6636k2h-evm/66/debug/edma3_lld_drv_sample.ae66
Linking with library ti.csl:./lib/k2h/c66/release/ti.csl.ae66
Linking with library ti.drv.pcie:./lib/c66/release/ti.drv.pcie.profiling.ae66
Linking with library ti.utils.profiling:./lib/c66/release/ti.utils.profiling.ae66
Inside EDMA3 Drv getLibs
will link with ti.sdo.edma3.drv:lib/66/debug/edma3_lld_drv.ae66
Inside EDMA3 RM getLibs
will link with ti.sdo.edma3.rm:lib/tci6636k2h-evm/66/debug/edma3_lld_rm.ae66
Starting build of library sources ...
making C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/k2h/c66/bios/src/sysbios/sysbios.ae66 ...
gmake[1]: Entering directory `C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/k2h/c66/bios/src/sysbios'
gmake[1]: Nothing to be done for `all'.
gmake[1]: Leaving directory `C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/k2h/c66/bios/src/sysbios'
Build of libraries done.
cle66 package/cfg/pcie_sample_wSoCFile_pe66.c ...
'Finished building: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/k2h/c66/bios/pcie_sample_wSoCFile.cfg'
' '
gmake[1]: Leaving directory 'C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject/Debug'
'Building file: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/soc/k2h/src/pcie_soc.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6600 --include_path="C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject" --include_path="C:/ti/pdk_k2hk_4_0_4/packages" --include_path="C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/src" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --define=DEVICE_K2H --diag_wrap=off --diag_warning=225 --display_error_number --exit_hook=ti_utils_exit --exit_parm=address --entry_parm=address --entry_hook=ti_utils_entry --preproc_with_compile --preproc_dependency="pcie_soc.d" --cmd_file="configPkg/compiler.opt" "C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/soc/k2h/src/pcie_soc.c"
'Finished building: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/soc/k2h/src/pcie_soc.c'
' '
'Building file: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/commonEDMA.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6600 --include_path="C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject" --include_path="C:/ti/pdk_k2hk_4_0_4/packages" --include_path="C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/src" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --define=DEVICE_K2H --diag_wrap=off --diag_warning=225 --display_error_number --exit_hook=ti_utils_exit --exit_parm=address --entry_parm=address --entry_hook=ti_utils_entry --preproc_with_compile --preproc_dependency="commonEDMA.d" --cmd_file="configPkg/compiler.opt" "C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/commonEDMA.c"
'Finished building: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/commonEDMA.c'
' '
'Building file: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/PCIeEDMAselector.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6600 --include_path="C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject" --include_path="C:/ti/pdk_k2hk_4_0_4/packages" --include_path="C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/src" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --define=DEVICE_K2H --diag_wrap=off --diag_warning=225 --display_error_number --exit_hook=ti_utils_exit --exit_parm=address --entry_parm=address --entry_hook=ti_utils_entry --preproc_with_compile --preproc_dependency="PCIeEDMAselector.d" --cmd_file="configPkg/compiler.opt" "C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/PCIeEDMAselector.c"
'Finished building: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/PCIeEDMAselector.c'
' '
'Building file: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/PCIeDMA.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6600 --include_path="C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject" --include_path="C:/ti/pdk_k2hk_4_0_4/packages" --include_path="C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/src" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --define=DEVICE_K2H --diag_wrap=off --diag_warning=225 --display_error_number --exit_hook=ti_utils_exit --exit_parm=address --entry_parm=address --entry_hook=ti_utils_entry --preproc_with_compile --preproc_dependency="PCIeDMA.d" --cmd_file="configPkg/compiler.opt" "C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/PCIeDMA.c"
'Finished building: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/EDMA/PCIeDMA.c'
' '
'Building file: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/src/pcie_sample.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6600 --include_path="C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject" --include_path="C:/ti/pdk_k2hk_4_0_4/packages" --include_path="C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/src" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --define=DEVICE_K2H --diag_wrap=off --diag_warning=225 --display_error_number --exit_hook=ti_utils_exit --exit_parm=address --entry_parm=address --entry_hook=ti_utils_entry --preproc_with_compile --preproc_dependency="pcie_sample.d" --cmd_file="configPkg/compiler.opt" "C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/src/pcie_sample.c"
'Finished building: C:/ti/pdk_k2hk_4_0_4/packages/ti/drv/pcie/example/sample/src/pcie_sample.c'
' '
'Building target: PCIE_K2H_wSoCFile_C66BiosExampleProject.out'
'Invoking: C6000 Linker'
"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6600 -g --define=DEVICE_K2H --diag_wrap=off --diag_warning=225 --display_error_number --exit_hook=ti_utils_exit --exit_parm=address --entry_parm=address --entry_hook=ti_utils_entry -z -m"PCIE_K2H_wSoCFile_C66BiosExampleProject.map" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/lib" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3/include" --reread_libs --diag_wrap=off --warn_sections --display_error_number --xml_link_info="PCIE_K2H_wSoCFile_C66BiosExampleProject_linkInfo.xml" --rom_model -o "PCIE_K2H_wSoCFile_C66BiosExampleProject.out" "./PCIeDMA.obj" "./PCIeEDMAselector.obj" "./commonEDMA.obj" "./pcie_sample.obj" "./pcie_soc.obj" -l"configPkg/linker.cmd" -llibc.a
<Linking>
'Finished building target: PCIE_K2H_wSoCFile_C66BiosExampleProject.out'
' '
C:/ti/pdk_k2hk_4_0_4/packages/pdkAppImageCreate.bat C:/ti/pdk_k2hk_4_0_4/packages C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3 C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject/Debug PCIE_K2H_wSoCFile_C66BiosExampleProject K2H dsp
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>set PDK_PATH=C:/ti/pdk_k2hk_4_0_4/packages
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>set CG_TOOL_PATH=C:/ti/ccsv7/tools/compiler/ti-cgt-c6000_8.1.3
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>set APP_PATH=C:/Users/keunsu/workspace_v7/PCIE_K2H_wSoCFile_C66BiosExampleProject/Debug
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>set APP_NAME=PCIE_K2H_wSoCFile_C66BiosExampleProject
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>set SOC=K2H
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>set PROCESSOR=dsp
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>if K2H == AM437x (goto SOC_AM3_AM4 )
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>if K2H == AM335x (goto SOC_AM3_AM4 )
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>if K2H == AM572x (goto SOC_AM57XX )
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>if K2H == AM571x (goto SOC_AM57XX )
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>else (
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>echo ERROR: Invalid SOC
ERROR: Invalid SOC
C:\Users\keunsu\workspace_v7\PCIE_K2H_wSoCFile_C66BiosExampleProject\Debug>goto ENDSCRIPT
' '
'else' is not recognized as an internal or external command,
operable program or batch file.
**** Build Finished ****