/home/jvsd/dvsdk_1_40_02_33/dmai_1_10_00_06/packages/ti/sdo/dmai/linux/dm6467/Blend.c
build failed as it Could not find the include file:
#include <asm/arch/davinci_vdce.h>
should it be (since I do find .h's in the target/...../lsp...../asm-arm/arch-davinci directory>
<asm-arm/arch-davinci/davinci_vdce.h>
but it fails at other places that have <asm/arch/(other).h'
I did not want to keep making wholesale changes to code and recompining since I felt there might be wrong or there may be some fix available which I dont know about.
Thanks,
Jawa