Hi, all.
I've test the 1080P encoder on DM6467, but when the image height is set to 1080, the encoder is failed to be created. But from the encoder user guide, the encoder can pad the height when not a multiple of 16. So I'd like to ask whether the encoder support really 1920x1080 encoding or just a 1920x1072 encoder?
Thanks