Hi,
i obtain this CMEM error executing av_server on DM365IPNC.
what could be wrong? it seems to be enough heap memory allocated
CMEMK Error: ioctl: failed to allocate heap buffer of size 0x4c9400
CMEM Error: allocHeap: ioctl CMEM_IOCALLOCHEAP failed: -1
this is the cmem message when i load the module
CMEMK module: built on Jul 23 2010 at 15:45:16
Reference Linux version 2.6.18
File /home/software/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
allocated heap buffer 0xc5000000 of size 0x4800000
CMEM Range Overlaps Kernel Physical - allowing overlap
CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83800000)
cmemk initialized
Regards
Andrea