Part Number: DM388
Tool/software: Linux
Dear DM388 team,
customer is trying to leverage the new SDK on the DM388 Appro camera hardware.
They got the new SDK running, but they have an issue; it seems that Ethernet PHY is misconfigured both in U-Boot and Kernel.
U-Boot:
Could not get PHY for cpsw: addr 25
Kernel:
[ 213.463904] net eth0: initializing cpsw version 1.10 (0) [ 213.471170] net eth0: initialized cpsw ale version 1.3 [ 213.478270] net eth0: phy "/ocp/ethernet@4a100000/mdio@4a100800/ethernet-phy@25" not found on slave 0 [ 213.487564] libphy: PHY not found [ 213.490986] net eth0: phy "" not found on slave 1, err -19 [ 213.515866] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
Is there any quick fix, like new dtb file for Kernel?
Thanks for your prompt help,
Kind regards,
Giuseppe