Other Parts Discussed in Thread: TMDSEMU110-U, TMDSEMU200-U, TMDSEMU560V2STM-UE, TMDSEMU560V2STM-U
Tool/software: Code Composer Studio
Hi,
I new to DSP and learning to work with TMS320C6748, I followed all the steps given to run demo. But after setting the baud rate in tera term, and powering the board Iam not getting any message on the console as it's shown in the instructions.
I even tried to connect it to through CCS but there also getting some errors connecting the board, I think this is because iam not using any emulator.
My questions are :
1. Do I need emulators to run demos through TeraTerm.
2. To work in CCS I need emulator, which ones will work with TMS320C7648, or which emulator is good.
3. To work on CCS using emulator can anyone provide the steps. ( I searched on YouTube/ web but I didn't find any detailed explanation.)
It would be of great help if I could get any help in this...
,
Thanks.