Part Number: 66AK2H12
Hello,
In my custom board, I have connected 66AK2H12 and two M88E6131 gigabit ethernet switches SGMII0,SGMII1 respectively.
SGMII 2 of processor is connected to M88E1111 gigabit ethernet Phy.
I have got through-put between processor and both switches (66.7 KiB/s constantly) in u-boot 2013 version whereas
gigabit phy and processor is giving around 2.2 MiB/s .
I have made configuration for switches and processor as MAC MAC FORCED in which processor is the SGMII master in u-boot.
For your info, MAC MAC AUTONEG config is not working fine.
I measured the waveforms of TX and RX which looks good.
Also I have verified the statistics counters on processor and switches which also looks fine (No errors or packet drops).
My question is whether any additional things have to be taken care for SGMII MAC MAC configurations?
Do i need to do any extra things with serdes init settings (com, cmu,lane settings) such as boost,attenuation?
Let me know if any further details re required.
It is very much urgent to resolve the issue. Kindly help on this.
P.S: I am not sure which document the com,cmu,lanes are being referred in u-boot as well as CSL serdes settings.
Because the serdes settings is not matching with SPRUHO3A.
Regards,
Sivanantham