This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA744: PCIe output REFCLK electrical compatibility

Part Number: DRA744

Referring to the datasheet of Jacinto 6, paragraph 8.5.6.3 ("LJCB_REFN / P Connections") presents the ability to configure two modes of operation for the PCIe clock:

  • External Mode Refclk
  • Output Mode Refclk

About the latter option:

“In Output REFCLK Mode, the 100MHz clock from the Device’s DPLL_PCIE_REF should be output on the Device’s ljcb_clkn / ljcb_clkp pins and used as the HCSL REFCLK by the link partner. External nearside termination to ground described in Table 8-29 is required on both of the ljcb_clkn / ljcb_clkp outputs in this mode.”

 

In our application the link partner is a WiFi module with LVPECL clock input:

  • is it possible to match a HCSL driver with a LVPECL input by mean of a passive network?
  • in this case, how much would be the max trace length?