This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2E: ETHERNET CAMERA

Part Number: TDA2E

Tool/software: Linux


 We want to place the TDA2x board on the car dashboard, and the camera in front of the car. So, there will be at least 5-6 m distance between the camera and the TDA2x board. We already tested by sending a video from PC to board through Ethernet port via network_tx tool in PC. So we wanted to use IP camera which can stream the video through the Ethernet port, using the specific IP of the board.
Please advice.

Regarding display:
Other then LCD display, can we use any other display which can support a distance around 1-2 m?
We already have a LCD display, but it does support short distance.
Whether HDMI (length of 2m)can be used for display purpose?