This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: CAN0 issue

Part Number: PROCESSOR-SDK-AM335X

Hi,

I am experiencing some weird behavior with can0 and am hoping someone can provide some insight. I have validated some sensor software using can1 successfully. However, when using can0 what I have seen is the following:

  • When connected to a can transceiver at 250k or 500k, the tx line oscillates at around 19kHz and won't stop without bringing down the bus (ip link set can0 down/up).
  • When not connected to a can transceiver, or when connected to a can transceiver at 125k, I can send only one can frame. Further attempts don't show up on the can tx line with out bringing the bus down and back up again.
  • The OS shows no errors as far as accessing can0.

Has anyone seen or heard of anything similar to this problem?

Thanks,
Tom