Hi,
I changed the uboot delay to 0 and I can not stopped in uBoot any more, so I reset my uboot envrionment variable to all zeros by doing the following: dd if=/dev/zero of=/dev/mtdblock2’. Now I try to set my boot environment variables to be able to boot up with 2 choices: 1) boot up from flash, 2) bootup to my Host via NFS using tftp, but neither of them were succeed. Boot up using TFTP to my host could not get the correct ip address: it shouwed the TFTP from server 0.10.17.100 which is wrong, but target IP address is 10.17.100.56 is correct, and boot up to flash got the folloiwng before Kernel PANIC:
List of all partitions:
1f00 512 mtdblock0 (driver?)
1f01 1792 mtdblock1 (driver?)
1f02 256 mtdblock2 (driver?)
1f03 5120 mtdblock3 (driver?)
1f04 254464 mtdblock4 (driver?)
No filesystem could mount root, tried: ext3 ext2 vfat msdos
I have the following environment varaibles set for uboot, did I miss any setups?
bootdelay=10
baudrate=115200
netmask=255.255.254.0
bootfile="uImage"
nfshost="10.17.100.173"
get_kernel=run nand_kernel
nand_kernel=nand read.i 0x80000000 280000 220000
myBootArgs="console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=10.17.100.173:/home/azhang/nfsdir/timeSysNfs,
nolock mem=99M mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y"
serverip="10.17.100.173"
myBoot=setenv bootargs $(myBootArgs);dhcp;bootm
ethaddr=00:50:C2:7E:90:C6
bootargs_fs=mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootstype=jffs2 mpurate=600
boot_fs=run get_kernel;setenv bootargs $(bootargs_fs); bootm
bootcmd=run boot_fs
ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):$(hostname):eth0:on
stdin=serial
stdout=serial
stderr=serial