Other Parts Discussed in Thread: TVP7002
Hi, I'm a new user of the 6467 DVEVM.
I've been trying to modify the "encode" demo that is included with the DVSDK to allow encoding of 1080 video. Simply changing the maxHeight and maxWidth parameters in the VIDENC1_Params struct is apparently insufficient, as the Venc1_create() call keeps failing to create the encoder. I've also tried rounding these to the nearest multiple of 16, with similar lack of success. What else is required to successfully create the encoder for 1920x1080 video? I was under the impression that the DM6467 was capable of encoding and decoding HD video at 1080 resolution, but the demos all seem to restrict to <= 720. The Venc1_create() call just fails without much useful information.
Has anyone had any success in encoding 1080 video on this platform?
I appreciate whatever help you can provide,
Doug Reher