Part Number: 430BOOST-C55AUDIO1
Hello, while putting mp3 files on the SD card some were not copied well and apparently corrupted, then the ACTBP not working well. I made a backup of the contents of the SD card with dd in linux, then put the contents back on the SD card but it did not work anymore. I read in the forums about the problem, and is that the MP3 CODEC is protected. Is there any way I can get an SD card from TI or I can put the MP3 CODEC, I thought it was in my backup, but apparently not. Regards!
Raul