This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error: Failed to create video h264fhdvenc encoder:



I am now trying  to integrate the H264fhdvenc into my sever. I have successfully finished this step. But when I try to create an instance, the algInit call failed. [DSP]

 

 

  • hello,

    Can you outline: -

    - vers # of the codec

    - where it came from (URL)

    - what u did to add/integrate it

    Cheers, Alan

  • thanks AC.

    version:

                       dm6467_h264fhdvenc_01_10_00_26_production

                      dm6467_hdvicp_1_01_017_production

                    Code Generation Tool version 6.0.8
    −             Codec Engine (CE) version 2.10.01
    −             DSP/BIOSTM version 5.31

       dvsdk_2_00_00_22

     

    I download this codec from ti website, but I have forget the url

     

    The method that I integrated the codec into my encoder server is as follows:


    First, I just replace the old hpcip lib with the new hpvip——1_01_017 ,and copy  h264fhdvenc codec to  combos/packages/ti/sdo/codecs

    Second, I modify the .conf and .tcf files of my encoder . at http://e2e.ti.com/forums/t/12408.aspx

                The key pionts as:

                EDMA3.maxTccs[0] =  49;
               EDMA3.maxEdmaChannels[0] = 49;

               : 2Mode: "64k"

                bios.MEM.instance("IRAM").heapSize = 0x10000;   //64k

    Third,
    I start to modify the encoder demo, which is to change the IH264ENC_Params H264ENC_DynamicParams into the new   IH264FHDVENC_Params、IH264FHDVENC_DynamicParams. After this, I create an encoder instance

     

     

  • zhangke said:

    version:

                       dm6467_h264fhdvenc_01_10_00_26_production

                      dm6467_hdvicp_1_01_017_production

                    Code Generation Tool version 6.0.8
    −             Codec Engine (CE) version 2.10.01
    −             DSP/BIOSTM version 5.31

       dvsdk_2_00_00_22

    Looks like you based these versions on the codec data sheet (which is reasonable). However the codec datasheet typically shows testing in isolation (outside of the DVSDK). Hence the versions are often different than the DVSDK. I suggest u revert to the versions of tools required by DVSDK 2.0. For example BIOS 5.31 is old. DVSDK 2.0 shipped w/ 5.33.03. I suspect you get a bunch of warnings in the build due to this.You should also use CGT >= 6.0.21

    zhangke said:
    First, I just replace the old hpcip lib with the new hpvip——1_01_017

    Make sure you really nuke the previous HDVICP lib to ensure no build remnants are left over and do a make clean.

    Also (once I found the codec you mentioned) you should look at codecs\h264fhdenc\H264FHDVENC.xdc - it has several config params - they'll all need set on the application (Arm) side - looks like there are some additional params .v. prev h264enc which is why I mention this.

    Finally codec params are often the issue that prevents successful creation. Suggest u copy the params provided in default Client app/ then take it forward from there.

    Cheers, Alan

     

  • Thanks AC
       I have been reverted the versions of the tools as follows:
         bios_5_33_03
         cg6x_6_0_21
       I deleted the previous library ,then copy hdvip_1_01_017
       codec to  combos/packages/ti/sdo/codecs, then "make clean ,make" to  re-build server without any warnings,
       I confirm that these is no problem.
      
       codec params set as:
        const VIDENC1_Params Venc1_Params_DEFAULT = {
        sizeof(VIDENC1_Params),           /* size */
        XDM_DEFAULT,                      /* encodingPreset */
        IVIDEO_LOW_DELAY,                 /* rateControlPreset */
        720,                              /* maxHeight */
        1280,                             /* maxWidth */
        30000,                            /* maxFrameRate */
        6000000,                          /* maxBitRate */
        XDM_BYTE,                         /* dataEndianness */
        0,                                /* maxInterFrameInterval */
        XDM_YUV_420P,                     /* inputChromaFormat */
        IVIDEO_PROGRESSIVE,               /* inputContentType */
        XDM_CHROMA_NA                     /* reconChromaFormat */


      but i don't know how to set on the application (Arm) side .I configed these params in encoder server
      's encoder.conf as
        H264FHDVENC.alg.codeSection  = "DDR2";
        H264FHDVENC.alg.intMemSection ="DDR2";
        H264FHDVENC.alg.udataSection = "DDR2";
        H264FHDVENC.alg.dataSection = "DDR2";
        H264FHDVENC.alg.umap1Section = "IRAM";
     
      However, there are still problems!Whether there is reference documentation about how to use the H264fhdvenc.

  • hello,

    Hopefully one of the developers can pitch in since I'm on vacation next week.

    1 point that comes to mind - the "intMemSection" parameter in the cfg file - that implies internal memory - which implies that perhaps internal memory is required for this section (possibly done via memory overlays etc). I have seen other codecs which did this for performance reasons. So if feasible try setting that to "IRAM".

    Make sure you double check the params you're using .v. the supplied Client/ application - this would at least get you started with a "known good".

    I'd also suggest you post the latest error msg you are getting.

    Regards, Alan

  • thank u for your suggestions, wish you a good vercation !
    I have read thethe params provided in default Client app. So I changed some params as follows:

    H264FHDVENC.alg.umap1Section = "KLD1_UMAP1";
    H264FHDVENC.alg.intMemSection ="IRAM";

    But still, it can't work.
    Here is the error msg:


    @0,165,616us: [+4 T:0x4001f950 S:0xbe8dca8c] OG - Global_init> This program was built with the following packages:
    @0,166,246us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package gnu.targets.rts470MV (/home/zhangke/dvsdk_2_00_00_22/xdctools_3_10_03/packages/gnu/targets/rts470MV/) [1,0,0,0,1225517438755]
    @0,166,471us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.codecs.h264fhdvenc (/home/zhangke/dvsdk_2_00_00_22/dm6467_dvsdk_combos_2_05/packages/ti/sdo/codecs/h264fhdvenc/) [1,0,0,1369825346000]
    @0,166,622us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.global (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/global/) [1,0,0,1240276693464]
    @0,166,765us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.xdais.dm (/home/zhangke/dvsdk_2_00_00_22/xdais_6_23/packages/ti/xdais/dm/) [1,0,5,1236972452910]
    @0,166,955us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.utils.trace (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/utils/trace/) [1,0,0,1240266922890]
    @0,167,098us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.utils.xdm (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/utils/xdm/) [1,0,2,1240276919490]
    @0,167,312us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package dsplink.gpp (/home/zhangke/dvsdk_2_00_00_22/dsplink-1_61_03-prebuilt/packages/dsplink/gpp/) [5,0,0,1239931267000]
    @0,167,455us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.linuxutils.cmem (/home/zhangke/dvsdk_2_00_00_22/linuxutils_2_23_01/packages/ti/sdo/linuxutils/cmem/) [2,2,0,1240253001679]
    @0,167,598us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.xdais (/home/zhangke/dvsdk_2_00_00_22/xdais_6_23/packages/ti/xdais/) [1,2,1,1236972427008]
    @0,167,734us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.node (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/node/) [1,0,0,1240276734858]
    @0,167,869us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.fc.global (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/global/) [1,0,0,1240266696499]
    @0,168,004us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.fc.dman3 (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/dman3/) [1,0,4,1240266658662]
    @0,168,143us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.fc.memutils (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/memutils/) [1,0,0,1240266801007]
    @0,168,281us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.fc.acpy3 (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/acpy3/) [1,0,4,1240266659108]
    @0,168,417us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package gnu.targets (/home/zhangke/dvsdk_2_00_00_22/xdctools_3_10_03/packages/gnu/targets/) [1,0,1,1225517427930]
    @0,168,553us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.catalog.c470 (/home/zhangke/dvsdk_2_00_00_22/xdctools_3_10_03/packages/ti/catalog/c470/) [1,0,1,0,0]
    @0,168,689us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.catalog.c6000 (/home/zhangke/dvsdk_2_00_00_22/xdctools_3_10_03/packages/ti/catalog/c6000/) [1,0,0,0,0]
    @0,168,827us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.platforms.evmDM6467 (/home/zhangke/dvsdk_2_00_00_22/xdctools_3_10_03/packages/ti/platforms/evmDM6467/) [1,0,0,0,0]
    @0,168,961us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.osal (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/osal/) [2,0,2,1240276730877]
    @0,169,096us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.osal.linux (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/osal/linux/) [2,0,1,1240276736840]
    @0,169,238us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.ipc (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/ipc/) [2,0,1,1240276698961]
    @0,169,477us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.ipc.dsplink (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/ipc/dsplink/) [2,0,1,1240276714152]
    @0,169,695us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.alg (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/alg/) [1,0,1,1240276276798]
    @0,169,855us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/) [1,0,6,1240276276491]
    @0,169,998us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.video1 (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/video1/) [1,0,2,1240276935900]
    @0,170,140us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.codecs.h264fhdvenc.ce (/home/zhangke/dvsdk_2_00_00_22/dm6467_dvsdk_combos_2_05/packages/ti/sdo/codecs/h264fhdvenc/ce/) [1,0,0,1369825346000]
    @0,170,279us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.speech (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/speech/) [1,0,2,1240276762193]
    @0,170,415us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.speech1 (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/speech1/) [1,0,1,1240276763928]
    @0,170,549us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.audio (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/audio/) [1,0,2,1240276296374]
    @0,170,685us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.audio1 (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/audio1/) [1,0,1,1240276296900]
    @0,170,823us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.video (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/video/) [1,0,3,1240276930771]
    @0,170,958us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.video2 (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/video2/) [1,0,2,1240276933444]
    @0,171,095us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.image (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/image/) [1,0,3,1240276700525]
    @0,171,235us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.image1 (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/image1/) [1,0,1,1240276698808]
    @0,171,372us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.dmai (/home/zhangke/dvsdk_2_00_00_22/dmai_1_20_00_06/packages/ti/sdo/dmai/) [1,0,0,1369818363000]
    @0,171,511us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.simplewidget (/home/zhangke/dvsdk_2_00_00_22/dvsdk_demos_2_00_00_07/packages/ti/sdo/simplewidget/) []
    @0,171,647us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.bioslog (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/bioslog/) [1,0,1,1240276303166]
    @0,171,781us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package ti.sdo.ce.utils.trace (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/utils/trace/) [1,0,1,1240276915917]
    @0,171,919us: [+4 T:0x4001f950 S:0xbe8dca8c] OG -     package encode_config (/home/zhangke/dvsdk_2_00_00_22/dvsdk_demos_2_00_00_07/dm6467/encode/encode_config/) []
    @0,358,805us: [+0 T:0x4001f950 S:0xbe8dca94] OG - Global_atexit> enter (fxn=0x30b70)
    @0,359,713us: [+0 T:0x4001f950 S:0xbe8dca94] OG - Global_atexit> enter (fxn=0x2ffbc)
    @0,360,480us: [+0 T:0x4001f950 S:0xbe8dca64] OM - Memory_alloc> Enter(0x18)
    @0,360,675us: [+0 T:0x4001f950 S:0xbe8dca64] OM - Memory_alloc> return (0x600f0)
    @0,362,046us: [+0 T:0x4001f950 S:0xbe8dca84] OG - Global_atexit> enter (fxn=0x2deec)
    @0,362,590us: [+0 T:0x4001f950 S:0xbe8dca5c] OM - Memory_alloc> Enter(0x18)
    @0,363,281us: [+0 T:0x4001f950 S:0xbe8dca5c] OM - Memory_alloc> return (0x60140)
    @0,363,461us: [+0 T:0x4001f950 S:0xbe8dca7c] OG - Global_atexit> enter (fxn=0x2cd98)
    @0,363,959us: [+0 T:0x4001f950 S:0xbe8dca84] OG - Global_atexit> enter (fxn=0x2f620)
    @0,365,048us: [+0 T:0x4001f950 S:0xbe8dca7c] ti.sdo.ce.osal.Sem - Sem_create> count: 0
    @0,365,235us: [+0 T:0x4001f950 S:0xbe8dca64] OM - Memory_alloc> Enter(0x14)
    @0,365,392us: [+0 T:0x4001f950 S:0xbe8dca64] OM - Memory_alloc> return (0x601c0)
    @0,365,565us: [+0 T:0x4001f950 S:0xbe8dca7c] ti.sdo.ce.osal.Sem - Leaving Sem_create> sem[0x601c0]
    @0,365,776us: [+0 T:0x4001f950 S:0xbe8dca7c] ti.sdo.ce.osal.Sem - Sem_create> count: 0
    @0,365,924us: [+0 T:0x4001f950 S:0xbe8dca64] OM - Memory_alloc> Enter(0x14)
    @0,366,072us: [+0 T:0x4001f950 S:0xbe8dca64] OM - Memory_alloc> return (0x601d8)
    @0,366,215us: [+0 T:0x4001f950 S:0xbe8dca7c] ti.sdo.ce.osal.Sem - Leaving Sem_create> sem[0x601d8]
    @0,366,354us: [+0 T:0x4001f950 S:0xbe8dca64] OM - Memory_alloc> Enter(0x18)
    @0,366,495us: [+0 T:0x4001f950 S:0xbe8dca64] OM - Memory_alloc> return (0x601f0)
    @0,366,637us: [+0 T:0x4001f950 S:0xbe8dca5c] OT - Thread_create> Enter (fxn=0x2b570, attrs=0x0)
    @0,366,781us: [+0 T:0x4001f950 S:0xbe8dca44] OM - Memory_alloc> Enter(0x64)
    @0,366,924us: [+0 T:0x4001f950 S:0xbe8dca44] OM - Memory_alloc> return (0x60210)
    @0,367,703us: [+0 T:0x4001f950 S:0xbe8dca5c] OT - Thread_create> Exit (task=0x60210)
    @0,367,895us: [+0 T:0x4001f950 S:0xbe8dca94] OG - Global_atexit> enter (fxn=0x2af60)
    @0,368,070us: [+0 T:0x4001f950 S:0xbe8dca94] OG - Global_atexit> enter (fxn=0x2d2e4)
    @0,368,308us: [+0 T:0x4001f950 S:0xbe8dca7c] ti.sdo.ce.alg - ALG_init> Enter
    @0,368,460us: [+0 T:0x4001f950 S:0xbe8dca6c] OG - Global_atexit> enter (fxn=0x2abac)
    @0,368,615us: [+0 T:0x4001f950 S:0xbe8dca9c] ti.sdo.ce.alg - ALG_init> Exit
    @0,368,754us: [+0 T:0x4001f950 S:0xbe8dca94] OG - Global_atexit> enter (fxn=0x29fd8)
    @0,368,916us: [+0 T:0x4001f950 S:0xbe8dca6c] OM - Memory_alloc> Enter(0x18)
    @0,369,073us: [+0 T:0x4001f950 S:0xbe8dca6c] OM - Memory_alloc> return (0x603f0)
    @0,369,225us: [+0 T:0x4001f950 S:0xbe8dca94] OG - Global_atexit> enter (fxn=0x2fb10)
    @0,371,309us: [+1 T:0x40bc8490 S:0x40bc7d74] OP - daemon> thread created.
    @0,371,730us: [+0 T:0x40bc8490 S:0x40bc7d74] OP - getCmd_d> Enter (proc=0x40bc7de8)
    @0,371,903us: [+0 T:0x40bc8490 S:0x40bc7d54] ti.sdo.ce.osal.Sem - Entered Sem_pend> sem[0x601c0] timeout[0xffffffff]
    @1,352,476us: [+6 T:0x4001f950 S:0xbe8dca8c] CE - Engine_init> CE debugging on (CE_DEBUG=3; allowed CE_DEBUG levels: 1=min, 2=good, 3=max)
    @1,352,713us: [+0 T:0x4001f950 S:0xbe8dca7c] OG - Global_atexit> enter (fxn=0x2746c)
    @1,352,887us: [+0 T:0x4001f950 S:0xbe8dca5c] OM - Memory_alloc> Enter(0x18)
    @1,353,047us: [+0 T:0x4001f950 S:0xbe8dca5c] OM - Memory_alloc> return (0x60430)
    @1,353,197us: [+0 T:0x4001f950 S:0xbe8dca5c] OM - Memory_alloc> Enter(0x18)
    @1,353,347us: [+0 T:0x4001f950 S:0xbe8dca5c] OM - Memory_alloc> return (0x60450)
    @1,353,490us: [+0 T:0x4001f950 S:0xbe8dca5c] OM - Memory_alloc> Enter(0x18)
    @1,353,639us: [+0 T:0x4001f950 S:0xbe8dca5c] OM - Memory_alloc> return (0x60470)
    @1,353,848us: [+0 T:0x4001f950 S:0xbe8dca94] CS - Server_init()
    @1,353,998us: [+0 T:0x4001f950 S:0xbe8dca94] CS - Server_init> Global_useLinkArbiter = 0
    @1,354,144us: [+0 T:0x4001f950 S:0xbe8dca94] OG - Global_atexit> enter (fxn=0x2574c)
    @1,354,472us: [+0 T:0x4001f950 S:0xbe8dcaa4] OG - Global_atexit> enter (fxn=0x1318c)
    TraceUtil_start> note: CE_DEBUG env. var is set, so TraceUtil is not active (unset CE_DEBUG if you need TraceUtil)
    @2,346,440us: [+2 T:0x413c8490 S:0x413c7cb4] ti.sdo.dmai - [BufTab] Allocating BufTab for 8 buffers
    @2,347,430us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> Enter(0x1c2000)
    @2,347,611us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> Enter(size=1843200, align=-1, cached=FALSE, heap=FALSE)
    @2,348,118us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_alloc(1843200) = 0x41bc9000.
    @2,348,322us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_getPhys(0x41bc9000) = 0x88f21000.
    @2,348,480us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> Enter(virtAddr=0x41bc9000, size=1843200, physAddr=0x88f21000)
    @2,348,624us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> creating new contigBuf object
    @2,348,754us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> Enter(0x10)
    @2,348,894us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> return (0x60958)
    @2,349,033us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> returning: cb->phys=0x88f21000, cb->size=1843200, cb->virt=0x41bc9000
    @2,349,238us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> return (0x41bc9000)
    @2,349,482us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> return (0x41bc9000)
    @2,349,641us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x41bc9000, size=4)
    @2,349,791us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x41bc9000, size=4)
    @2,349,933us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> found in cb(Sc=0x41bc9000, Ec=0x41d8b000, Ss=0x41bc9000, Es=0x41bc9004, PSc=0x88f21000)
    @2,350,083us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> returning physAddr=0x88f21000
    @2,350,222us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> return (0x88f21000)
    @2,350,358us: [+2 T:0x413c8490 S:0x413c7c8c] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1843200 at 0x41bc9000 (0x88f21000 phys)
    @2,350,521us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> Enter(0x1c2000)
    @2,350,667us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> Enter(size=1843200, align=-1, cached=FALSE, heap=FALSE)
    @2,351,143us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_alloc(1843200) = 0x41f16000.
    @2,351,342us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_getPhys(0x41f16000) = 0x8b60b000.
    @2,351,495us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> Enter(virtAddr=0x41f16000, size=1843200, physAddr=0x8b60b000)
    @2,351,647us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> creating new contigBuf object
    @2,351,778us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> Enter(0x10)
    @2,351,920us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> return (0x609e0)
    @2,352,055us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> returning: cb->phys=0x8b60b000, cb->size=1843200, cb->virt=0x41f16000
    @2,352,202us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> return (0x41f16000)
    @2,352,340us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> return (0x41f16000)
    @2,352,476us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x41f16000, size=4)
    @2,352,613us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x41f16000, size=4)
    @2,352,751us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> found in cb(Sc=0x41f16000, Ec=0x420d8000, Ss=0x41f16000, Es=0x41f16004, PSc=0x8b60b000)
    @2,352,901us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> returning physAddr=0x8b60b000
    @2,353,037us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> return (0x8b60b000)
    @2,353,177us: [+2 T:0x413c8490 S:0x413c7c8c] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1843200 at 0x41f16000 (0x8b60b000 phys)
    @2,353,343us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> Enter(0x1c2000)
    @2,353,490us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> Enter(size=1843200, align=-1, cached=FALSE, heap=FALSE)
    @2,353,959us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_alloc(1843200) = 0x4230b000.
    @2,354,162us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_getPhys(0x4230b000) = 0x8b216000.
    @2,354,317us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> Enter(virtAddr=0x4230b000, size=1843200, physAddr=0x8b216000)
    @2,354,464us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> creating new contigBuf object
    @2,354,597us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> Enter(0x10)
    @2,354,741us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> return (0x60a68)
    @2,354,877us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> returning: cb->phys=0x8b216000, cb->size=1843200, cb->virt=0x4230b000
    @2,355,023us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> return (0x4230b000)
    @2,355,162us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> return (0x4230b000)
    @2,355,300us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x4230b000, size=4)
    @2,355,441us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x4230b000, size=4)
    @2,355,636us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> found in cb(Sc=0x4230b000, Ec=0x424cd000, Ss=0x4230b000, Es=0x4230b004, PSc=0x8b216000)
    @2,355,796us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> returning physAddr=0x8b216000
    @2,355,934us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> return (0x8b216000)
    @2,356,073us: [+2 T:0x413c8490 S:0x413c7c8c] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1843200 at 0x4230b000 (0x8b216000 phys)
    @2,356,237us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> Enter(0x1c2000)
    @2,356,383us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> Enter(size=1843200, align=-1, cached=FALSE, heap=FALSE)
    @2,356,860us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_alloc(1843200) = 0x42700000.
    @2,357,062us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_getPhys(0x42700000) = 0x8ae21000.
    @2,357,219us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> Enter(virtAddr=0x42700000, size=1843200, physAddr=0x8ae21000)
    @2,357,370us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> creating new contigBuf object
    @2,357,503us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> Enter(0x10)
    @2,357,646us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> return (0x60af0)
    @2,357,784us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> returning: cb->phys=0x8ae21000, cb->size=1843200, cb->virt=0x42700000
    @2,357,929us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> return (0x42700000)
    @2,358,065us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> return (0x42700000)
    @2,358,205us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x42700000, size=4)
    @2,358,348us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x42700000, size=4)
    @2,358,488us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> found in cb(Sc=0x42700000, Ec=0x428c2000, Ss=0x42700000, Es=0x42700004, PSc=0x8ae21000)
    @2,358,637us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> returning physAddr=0x8ae21000
    @2,358,772us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> return (0x8ae21000)
    @2,358,907us: [+2 T:0x413c8490 S:0x413c7c8c] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1843200 at 0x42700000 (0x8ae21000 phys)
    @2,359,066us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> Enter(0x1c2000)
    @2,359,215us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> Enter(size=1843200, align=-1, cached=FALSE, heap=FALSE)
    @2,359,773us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_alloc(1843200) = 0x42af5000.
    @2,359,980us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_getPhys(0x42af5000) = 0x8aa2c000.
    @2,360,136us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> Enter(virtAddr=0x42af5000, size=1843200, physAddr=0x8aa2c000)
    @2,360,289us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> creating new contigBuf object
    @2,360,423us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> Enter(0x10)
    @2,360,568us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> return (0x60b78)
    @2,360,706us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> returning: cb->phys=0x8aa2c000, cb->size=1843200, cb->virt=0x42af5000
    @2,360,851us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> return (0x42af5000)
    @2,360,987us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> return (0x42af5000)
    @2,361,123us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x42af5000, size=4)
    @2,361,263us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x42af5000, size=4)
    @2,361,404us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> found in cb(Sc=0x42af5000, Ec=0x42cb7000, Ss=0x42af5000, Es=0x42af5004, PSc=0x8aa2c000)
    @2,361,554us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> returning physAddr=0x8aa2c000
    @2,361,689us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> return (0x8aa2c000)
    @2,361,878us: [+2 T:0x413c8490 S:0x413c7c8c] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1843200 at 0x42af5000 (0x8aa2c000 phys)
    @2,362,053us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> Enter(0x1c2000)
    @2,362,207us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> Enter(size=1843200, align=-1, cached=FALSE, heap=FALSE)
    @2,362,680us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_alloc(1843200) = 0x42eea000.
    @2,362,880us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_getPhys(0x42eea000) = 0x8a637000.
    @2,363,035us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> Enter(virtAddr=0x42eea000, size=1843200, physAddr=0x8a637000)
    @2,363,187us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> creating new contigBuf object
    @2,363,320us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> Enter(0x10)
    @2,363,465us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> return (0x60c00)
    @2,363,603us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> returning: cb->phys=0x8a637000, cb->size=1843200, cb->virt=0x42eea000
    @2,363,747us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> return (0x42eea000)
    @2,363,884us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> return (0x42eea000)
    @2,364,020us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x42eea000, size=4)
    @2,364,163us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x42eea000, size=4)
    @2,364,301us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> found in cb(Sc=0x42eea000, Ec=0x430ac000, Ss=0x42eea000, Es=0x42eea004, PSc=0x8a637000)
    @2,364,452us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> returning physAddr=0x8a637000
    @2,364,589us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> return (0x8a637000)
    @2,364,725us: [+2 T:0x413c8490 S:0x413c7c8c] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1843200 at 0x42eea000 (0x8a637000 phys)
    @2,364,886us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> Enter(0x1c2000)
    @2,365,034us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> Enter(size=1843200, align=-1, cached=FALSE, heap=FALSE)
    @2,365,509us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_alloc(1843200) = 0x432df000.
    @2,365,713us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_getPhys(0x432df000) = 0x8a242000.
    @2,365,868us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> Enter(virtAddr=0x432df000, size=1843200, physAddr=0x8a242000)
    @2,366,017us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> creating new contigBuf object
    @2,366,151us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> Enter(0x10)
    @2,366,296us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> return (0x60c88)
    @2,366,433us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> returning: cb->phys=0x8a242000, cb->size=1843200, cb->virt=0x432df000
    @2,366,579us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> return (0x432df000)
    @2,366,714us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> return (0x432df000)
    @2,366,852us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x432df000, size=4)
    @2,366,995us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x432df000, size=4)
    @2,367,135us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> found in cb(Sc=0x432df000, Ec=0x434a1000, Ss=0x432df000, Es=0x432df004, PSc=0x8a242000)
    @2,367,284us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> returning physAddr=0x8a242000
    @2,367,419us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> return (0x8a242000)
    @2,367,554us: [+2 T:0x413c8490 S:0x413c7c8c] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1843200 at 0x432df000 (0x8a242000 phys)
    @2,367,716us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> Enter(0x1c2000)
    @2,367,863us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> Enter(size=1843200, align=-1, cached=FALSE, heap=FALSE)
    @2,368,398us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_alloc(1843200) = 0x436d4000.
    @2,368,603us: [+4 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> CMEM_getPhys(0x436d4000) = 0x89e4d000.
    @2,368,759us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> Enter(virtAddr=0x436d4000, size=1843200, physAddr=0x89e4d000)
    @2,368,911us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> creating new contigBuf object
    @2,369,042us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> Enter(0x10)
    @2,369,191us: [+0 T:0x413c8490 S:0x413c7bcc] OM - Memory_alloc> return (0x60d10)
    @2,369,327us: [+1 T:0x413c8490 S:0x413c7be4] OM - Memory__addContigBuf> returning: cb->phys=0x89e4d000, cb->size=1843200, cb->virt=0x436d4000
    @2,369,584us: [+0 T:0x413c8490 S:0x413c7c2c] OM - Memory_contigAlloc> return (0x436d4000)
    @2,369,732us: [+0 T:0x413c8490 S:0x413c7c74] OM - Memory_alloc> return (0x436d4000)
    @2,369,876us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> Enter(virtAddr=0x436d4000, size=4)
    @2,370,019us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> Enter(virtAddr=0x436d4000, size=4)
    @2,370,164us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> found in cb(Sc=0x436d4000, Ec=0x43896000, Ss=0x436d4000, Es=0x436d4004, PSc=0x89e4d000)
    @2,370,314us: [+1 T:0x413c8490 S:0x413c7c54] OM - Memory__getPhysicalAddress> returning physAddr=0x89e4d000
    @2,370,451us: [+0 T:0x413c8490 S:0x413c7c54] OM - Memory_getBufferPhysicalAddress> return (0x89e4d000)
    @2,370,588us: [+2 T:0x413c8490 S:0x413c7c8c] ti.sdo.dmai - [Buffer] Alloc Buffer of size 1843200 at 0x436d4000 (0x89e4d000 phys)
    @2,371,062us: [+0 T:0x41bc8490 S:0x41bc7c84] CE - Engine_open> Enter('encode', 0x0, 0x41bc7cf4)
    @2,371,542us: [+0 T:0x41bc8490 S:0x41bc7c6c] OM - Memory_alloc> Enter(0x2c)
    @2,371,718us: [+0 T:0x41bc8490 S:0x41bc7c6c] OM - Memory_alloc> return (0x60d48)
    @2,376,921us: [+0 T:0x41bc8490 S:0x41bc7c84] CE - rserverOpen('encodeCombo.x64P'), count = 0
    @2,377,079us: [+0 T:0x41bc8490 S:0x41bc7c4c] OP - Processor_create> Enter(imageName='encodeCombo.x64P', linkCfg='(null)', attrs=0x41bc7cd8)
    @2,378,611us: [+0 T:0x41bc8490 S:0x41bc7c34] OM - Memory_alloc> Enter(0x24)
    @2,378,809us: [+0 T:0x41bc8490 S:0x41bc7c34] OM - Memory_alloc> return (0x60d78)
    @2,378,962us: [+0 T:0x41bc8490 S:0x41bc7c2c] OP - doCmd> Enter (cmdId=1, proc=0x60d78)
    @2,379,110us: [+0 T:0x41bc8490 S:0x41bc7c1c] ti.sdo.ce.osal.Sem - Entered Sem_post> sem[0x601c0]
    @2,379,314us: [+0 T:0x41bc8490 S:0x41bc7c2c] ti.sdo.ce.osal.Sem - Leaving Sem_post> sem[0x601c0]
    @2,379,574us: [+0 T:0x41bc8490 S:0x41bc7c0c] ti.sdo.ce.osal.Sem - Entered Sem_pend> sem[0x601d8] timeout[0xffffffff]
    @2,379,776us: [+0 T:0x40bc8490 S:0x40bc7d54] ti.sdo.ce.osal.Sem - Leaving Sem_pend> sem[0x601c0] status[0]
    @2,379,948us: [+0 T:0x40bc8490 S:0x40bc7d74] OP - getCmd_d> Exit (result=1)
    @2,380,091us: [+0 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Enter(proc=0x60d78)
    @2,380,237us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Initializing DSP PROC...
    @2,380,383us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Using DspLink config data for entry #0 [server 'encodeCombo.x64P']
    @2,380,537us: [+0 T:0x40bc8490 S:0x40bc7d5c] OM - Memory_alloc> Enter(0x118)
    @2,380,690us: [+0 T:0x40bc8490 S:0x40bc7d5c] OM - Memory_alloc> return (0x60da0)
    @2,380,839us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Adding DSP segment #0 to Link configuration: name='DDR2', startAddress=0x8fa00000, sizeInBytes=0x400000, shared=1, syncd=0
    @2,381,010us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Adding DSP segment #1 to Link configuration: name='DSPLINKMEM', startAddress=0x8fe00000, sizeInBytes=0x100000, shared=1, syncd=0
    @2,381,180us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Adding DSP segment #2 to Link configuration: name='RESET_VECTOR', startAddress=0x8ff00000, sizeInBytes=0x80, shared=1, syncd=0
    @2,381,344us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Adding DSP segment #3 to Link configuration: name='DDRALGHEAP', startAddress=0x8ba00000, sizeInBytes=0x4000000, shared=0, syncd=0
    @2,381,567us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Adding DSP segment #4 to Link configuration: name='IRAM', startAddress=0x11818000, sizeInBytes=0x10000, shared=0, syncd=0
    @2,381,743us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> DODSPCTRL was=1; now=0
    @3,373,314us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Attaching to DSP PROC...
    @3,389,134us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Opening MSGQ pool...
    @3,389,947us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Loading encodeCombo.x64P on DSP (1 args)...
    @3,486,060us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Starting DSP PROC...
    @3,548,495us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> Opening remote transport...
    @3,554,218us: [+2 T:0x40bc8490 S:0x40bc7d74] OP - Processor_create_d> return (1)
    @3,554,412us: [+0 T:0x40bc8490 S:0x40bc7d64] ti.sdo.ce.osal.Sem - Entered Sem_post> sem[0x601d8]
    @3,554,613us: [+0 T:0x41bc8490 S:0x41bc7c0c] ti.sdo.ce.osal.Sem - Leaving Sem_pend> sem[0x601d8] status[0]
    @3,554,778us: [+0 T:0x41bc8490 S:0x41bc7c2c] OP - doCmd> Exit (result=1)
    @3,554,918us: [+0 T:0x41bc8490 S:0x41bc7c4c] OP - Processor_create> return (0x60d78)
    @3,555,057us: [+0 T:0x41bc8490 S:0x41bc7c84] CE - rserverOpen('encodeCombo.x64P'): 0x5f3a0 done.
    @3,555,207us: [+0 T:0x41bc8490 S:0x41bc7c6c] OM - Memory_alloc> Enter(0x24)
    @3,555,356us: [+0 T:0x41bc8490 S:0x41bc7c6c] OM - Memory_alloc> return (0x61010)
    @3,555,643us: [+0 T:0x41bc8490 S:0x41bc7c5c] OC - Comm_create> Enter(queueName='encode_1022_0', queue=0x60d58, attrs=0x0)
    @3,555,820us: [+0 T:0x41bc8490 S:0x41bc7c44] OM - Memory_alloc> Enter(0x4)
    @3,555,976us: [+0 T:0x41bc8490 S:0x41bc7c44] OM - Memory_alloc> return (0x61038)
    @3,556,418us: [+0 T:0x41bc8490 S:0x41bc7c5c] OC - Comm_create> return (0x61038)
    @3,556,607us: [+0 T:0x41bc8490 S:0x41bc7c64] OM - Memory_free> Enter(0x61010, 0x24)
    @3,556,825us: [+0 T:0x41bc8490 S:0x41bc7c64] OM - Memory_free> return (0x1)
    @3,556,986us: [+0 T:0x41bc8490 S:0x41bc7c64] OC - Comm_alloc> Enter(poolId=0x0, msg=0x60d64, size=576)
    @3,557,177us: [+0 T:0x41bc8490 S:0x41bc7c64] OC - Comm_alloc> msg=0x442d8880, returning (0)
    @3,557,330us: [+0 T:0x41bc8490 S:0x41bc7c4c] OC - Comm_locate> Enter(queueName='rmsq', queue=0x60d54)
    @3,557,672us: [+0 T:0x40bc8490 S:0x40bc7d74] ti.sdo.ce.osal.Sem - Leaving Sem_post> sem[0x601d8]
    @3,557,869us: [+0 T:0x40bc8490 S:0x40bc7d74] OP - getCmd_d> Enter (proc=0x40bc7de8)
    @3,558,023us: [+0 T:0x40bc8490 S:0x40bc7d54] ti.sdo.ce.osal.Sem - Entered Sem_pend> sem[0x601c0] timeout[0xffffffff]
    @3,558,406us: [+0 T:0x41bc8490 S:0x41bc7c4c] OC - Comm_locate> return (0)
    @3,558,590us: [+0 T:0x41bc8490 S:0x41bc7c84] CE - checkServer(0x60d48)
    @3,558,801us: [+0 T:0x41bc8490 S:0x41bc7c54] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,559,025us: [+0 T:0x41bc8490 S:0x41bc7c54] OC - Comm_put> return (0)
    @3,559,222us: [+0 T:0x41bc8490 S:0x41bc7c4c] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7cf0, timeout=-1)
    @3,559,617us: [+0 T:0x41bc8490 S:0x41bc7c4c] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
    @3,559,803us: [+0 T:0x41bc8490 S:0x41bc7c84] CE - rmsInit> RMS initialized(0x60d48); CE_DEBUG on, setting DSP trace mask to *+01234567,GT_prefix=12345,GT_time=3
    @3,559,969us: [+0 T:0x41bc8490 S:0x41bc7c5c] CE - Engine_setTrace> Enter(engine=0x60d48, mask='*+01234567,GT_prefix=12345,GT_time=3')
    @3,560,142us: [+1 T:0x41bc8490 S:0x41bc7c5c] CE - Engine_setTrace> Requesting DSP set trace ...
    @3,560,281us: [+0 T:0x41bc8490 S:0x41bc7c2c] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,560,482us: [+0 T:0x41bc8490 S:0x41bc7c2c] OC - Comm_put> return (0)
    @3,560,633us: [+0 T:0x41bc8490 S:0x41bc7c24] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7ca4, timeout=-1)
    @3,562,446us: [+0 T:0x41bc8490 S:0x41bc7c24] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
    @3,562,642us: [+0 T:0x41bc8490 S:0x41bc7c5c] CE - Engine_setTrace> return(0)
    @3,562,815us: [+0 T:0x41bc8490 S:0x41bc7bec] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,563,084us: [+0 T:0x41bc8490 S:0x41bc7bec] OC - Comm_put> return (0)
    @3,563,285us: [+0 T:0x41bc8490 S:0x41bc7be4] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7c84, timeout=-1)
    @3,563,590us: [+0 T:0x41bc8490 S:0x41bc7be4] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
    [DSP] @0,027,966tk: [+0 T:0x8ba0006c S:0x8ba03fe4] OG - Global_setSpecialTrace> enter(mask='*+01234567,GT_prefix=12345,GT_time=3')
    [DSP] @0,028,058tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG - Global_setSpecialTrace> This program was built with the following packages:
    [DSP] @0,028,118tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.targets.rts6000 (/home/zhangke/dvsdk_2_00_00_22/xdctools_3_10_03/packages/ti/targets/rts6000/) [1,0,0,0,1225517497925]
    [DSP] @0,028,201tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.codecs.h264fhdvenc (/home/zhangke/dvsdk_2_00_00_22/dm6467_dvsdk_combos_2_05/packages/ti/sdo/codecs/h264fhdvenc/) [1,0,0,1369825346000]
    [DSP] @0,028,291tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.codecs.hdvicp (/home/zhangke/dvsdk_2_00_00_22/dm6467_dvsdk_combos_2_05/packages/ti/sdo/codecs/hdvicp/) [1,0,0,1369825424000]
    [DSP] @0,028,383tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.global (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/global/) [1,0,0,1240266696499]
    [DSP] @0,028,468tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.edma3.rm (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/fctools/packages/ti/sdo/edma3/rm/) [1,3,4,1225865844769]
    [DSP] @0,028,555tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.ires.hdvicp (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/ires/hdvicp/) [1,0,1,1240266763264]
    [DSP] @0,028,643tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.utils.trace (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/utils/trace/) [1,0,0,1240266922890]
    [DSP] @0,028,729tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.rtdx (/home/zhangke/dvsdk_2_00_00_22/bios_5_33_03/packages/ti/rtdx/) [2,0,0,4,1219531643983]
    [DSP] @0,028,802tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.psl (/home/zhangke/dvsdk_2_00_00_22/bios_5_33_03/packages/ti/psl/) [5,0,0,0,0]
    [DSP] @0,028,869tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.bios (/home/zhangke/dvsdk_2_00_00_22/bios_5_33_03/packages/ti/bios/) [5,2,5,6,1227035764854]
    [DSP] @0,028,943tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.dskt2 (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/dskt2/) [1,0,4,1240266678055]
    [DSP] @0,029,026tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.hdintc (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/hdintc/) [1,0,4,1240266707594]
    [DSP] @0,029,111tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.memutils (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/memutils/) [1,0,0,1240266801007]
    [DSP] @0,029,197tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.ires.nullresource (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/ires/nullresource/) [1,0,0,1240266782634]
    [DSP] @0,029,289tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.rman (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/rman/) [2,0,0,1240266813533]
    [DSP] @0,029,372tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.edma3 (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/edma3/) [2,0,0,1240266681138]
    [DSP] @0,029,456tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.ires.edma3chan (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/ires/edma3chan/) [1,0,0,1240266737833]
    [DSP] @0,029,547tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.global (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/global/) [1,0,0,1240276693464]
    [DSP] @0,029,628tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.xdais.dm (/home/zhangke/dvsdk_2_00_00_22/xdais_6_23/packages/ti/xdais/dm/) [1,0,5,1236972452910]
    [DSP] @0,029,702tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.xdais (/home/zhangke/dvsdk_2_00_00_22/xdais_6_23/packages/ti/xdais/) [1,2,1,1236972427008]
    [DSP] @0,029,774tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.node (/home/zhangke/dvs@3,569,642us: [+0 T:0x41bc8490 S:0x41bc7bec] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,569,866us: [+0 T:0x41bc8490 S:0x41bc7bec] OC - Comm_put> return (0)
    @3,570,054us: [+0 T:0x41bc8490 S:0x41bc7be4] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7c84, timeout=-1)
    @3,570,360us: [+0 T:0x41bc8490 S:0x41bc7be4] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
    dk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/node/) [1,0,0,1240276734858]
    [DSP] @0,029,854tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.ipc.dsplink.dsp (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/ipc/dsplink/dsp/) [2,0,1,1240276720026]
    [DSP] @0,029,943tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.utils.xdm (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/utils/xdm/) [1,0,2,1240276919490]
    [DSP] @0,030,027tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.dman3 (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/dman3/) [1,0,4,1240266658662]
    [DSP] @0,030,110tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.fc.acpy3 (/home/zhangke/dvsdk_2_00_00_22/framework_components_2_23_01/packages/ti/sdo/fc/acpy3/) [1,0,4,1240266659108]
    [DSP] @0,030,194tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package dsplink.dsp (/home/zhangke/dvsdk_2_00_00_22/dsplink-1_61_03-prebuilt/packages/dsplink/dsp/) [1,4,0,1239931280000]
    [DSP] @0,030,273tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.bios.utils (/home/zhangke/dvsdk_2_00_00_22/biosutils_1_01_00/packages/ti/bios/utils/) [2,0,1,0,0]
    [DSP] @0,030,348tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.catalog.c6000 (/home/zhangke/dvsdk_2_00_00_22/xdctools_3_10_03/packages/ti/catalog/c6000/) [1,0,0,0,0]
    [DSP] @0,030,424tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.platforms.evmDM6467 (/home/zhangke/dvsdk_2_00_00_22/bios_5_33_03/packages/ti/platforms/evmDM6467/) [1,0,0,0,0]
    [DSP] @0,030,504tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.osal (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/osal/) [2,0,2,1240276730877]
    [DSP] @0,030,584tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.osal.bios (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/osal/bios/) [2,0,1,1240276734107]
    [DSP] @0,030,671tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.ipc (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/ipc/) [2,0,1,1240276698961]
    [DSP] @0,030,750tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.ipc.bios (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/ipc/bios/) [2,0,1,1240276705217]
    [DSP] @0,030,833tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.alg (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/alg/) [1,0,1,1240276276798]
    [DSP] @0,030,913tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/) [1,0,6,1240276276491]
    [DSP] @0,030,989tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.bioslog (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/bioslog/) [1,0,1,1240276303166]
    [DSP] @0,031,072tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.ce.video1 (/home/zhangke/dvsdk_2_00_00_22/codec_engine_2_23_01/packages/ti/sdo/ce/video1/) [1,0,2,1240276935900]
    [DSP] @0,031,153tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.codecs.h264fhdvenc.ce (/home/zhangke/dvsdk_2_00_00_22/dm6467_dvsdk_combos_2_05/packages/ti/sdo/codecs/h264fhdvenc/ce/) [1,0,0,1369825346000]
    [DSP] @0,031,245tk: [+4 T:0x8ba0006c S:0x8ba03fe4] OG -     package ti.sdo.servers.encode (/home/zhangke/dvsdk_2_00_00_22/dm6467_dvsdk_combos_2_05/packages/ti/sdo/servers/encode/) []
    [DSP] @0,031,325tk: [+0 T:0x8ba0006c S:0x8ba03fe4] OG - Global_setSpecialTrace> return
    [DSP] @0,033,975tk: [+0 T:0x8ba0006c S:0x8ba0402c] CR - processRmsCmd(0x8fe038a8, 4056): cmd = 5
    [DSP] @0,034,033tk: [+0 T:0x8ba0006c S:0x8ba0402c] CR - remote time = 0x0, trace buffer size = 4032
    [DSP] @0,049,715tk: [+0 T:0x8ba0006c S:0x8ba0402c] CR - processRmsCmd(0x8fe038a8, 4056): cmd = 5
    [DSP] @0,049,769tk: [+0 T:0x8ba0006c S:0x8ba0402c] CR - remote time = 0x0, trace buffer size = 4032
    @3,575,881us: [+0 T:0x41bc8490 S:0x41bc7c1c] CE - Engine_fwriteTrace> returning count [8114]
    @3,576,035us: [+0 T:0x41bc8490 S:0x41bc7c84] CE - Engine_open> return(396616)
    @3,576,240us: [+2 T:0x41bc8490 S:0x41bc7c0c] ti.sdo.dmai - [Venc1] Creating encoder h264fhdvenc for max 1280x720 bitrate 2000000 ratectrl 4
    @3,576,506us: [+0 T:0x41bc8490 S:0x41bc7be4] ti.sdo.ce.video1.VIDENC1 - VIDENC1_create> Enter (engine=0x60d48, name='h264fhdvenc', params=0x41bc7d2c)
    @3,576,693us: [+0 T:0x41bc8490 S:0x41bc7bb4] CV - VISA_create(0x60d48, 'h264fhdvenc', 0x41bc7d2c, 0x2496, 'ti.sdo.ce.video1.IVIDENC1')
    @3,576,853us: [+0 T:0x41bc8490 S:0x41bc7ab4] CV - VISA_create2(0x60d48, 'h264fhdvenc', 0x41bc7d2c, 0x3c, 0x2496, 'ti.sdo.ce.video1.IVIDENC1')
    @3,577,027us: [+0 T:0x41bc8490 S:0x41bc7a9c] OM - Memory_alloc> Enter(0x30)
    @3,577,182us: [+0 T:0x41bc8490 S:0x41bc7a9c] OM - Memory_alloc> return (0x61180)
    @3,577,325us: [+0 T:0x41bc8490 S:0x41bc7a3c] CE - Engine_createNode(0x60d48, 'h264fhdvenc', 2496, 0x41bc7d2c, 0x3c, 0x41bc7bac)
    @3,577,483us: [+0 T:0x41bc8490 S:0x41bc7a3c] CE - Engine> allocNode Enter(engine=0x60d48, impId='h264fhdvenc')
    @3,577,624us: [+0 T:0x41bc8490 S:0x41bc7a24] OM - Memory_alloc> Enter(0x20)
    @3,577,765us: [+0 T:0x41bc8490 S:0x41bc7a24] OM - Memory_alloc> return (0x61010)
    @3,577,924us: [+0 T:0x41bc8490 S:0x41bc7a3c] CE - Engine> allocNode(). Calling Comm_create(gppfromnode_1022_1, 0x61018, NULL)
    @3,578,074us: [+0 T:0x41bc8490 S:0x41bc7a14] OC - Comm_create> Enter(queueName='gppfromnode_1022_1', queue=0x61018, attrs=0x0)
    @3,578,224us: [+0 T:0x41bc8490 S:0x41bc79fc] OM - Memory_alloc> Enter(0x4)
    @3,578,370us: [+0 T:0x41bc8490 S:0x41bc79fc] OM - Memory_alloc> return (0x611b8)
    @3,578,812us: [+0 T:0x41bc8490 S:0x41bc7a14] OC - Comm_create> return (0x611b8)
    @3,579,007us: [+0 T:0x41bc8490 S:0x41bc7a1c] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,579,226us: [+0 T:0x41bc8490 S:0x41bc7a1c] OC - Comm_put> return (0)
    @3,579,463us: [+0 T:0x41bc8490 S:0x41bc7a14] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7ac4, timeout=-1)
    @3,612,156us: [+0 T:0x41bc8490 S:0x41bc7a14] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
    @3,612,425us: [+0 T:0x41bc8490 S:0x41bc7a14] OC - Comm_delete> Enter (comm=0x611b8)
    @3,613,016us: [+0 T:0x41bc8490 S:0x41bc79f4] OM - Memory_free> Enter(0x611b8, 0x4)
    @3,613,227us: [+0 T:0x41bc8490 S:0x41bc79f4] OM - Memory_free> return (0x1)
    @3,613,470us: [+0 T:0x41bc8490 S:0x41bc7a34] OC - Comm_delete> return
    @3,613,674us: [+0 T:0x41bc8490 S:0x41bc7a1c] OM - Memory_free> Enter(0x61010, 0x20)
    @3,613,852us: [+0 T:0x41bc8490 S:0x41bc7a1c] OM - Memory_free> return (0x1)
    @3,614,064us: [+6 T:0x41bc8490 S:0x41bc7a3c] CE - Engine_createNode> Remote node creation FAILED (0x80008008).
    @3,614,250us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,614,550us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> return (0)
    @3,614,818us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7a3c, timeout=-1)
    @3,615,184us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
    [DSP] @0,071,433tk: [+0 T:0x8ba0006c S:0x8ba0402c] CR - processRmsCmd(0x8fe038a8, 4056): cmd = 0
    [DSP] @0,071,492tk: [+0 T:0x8ba0006c S:0x8ba03f1c] OM - Memory_alloc> Enter(size=0x18)
    [DSP] @0,071,542tk: [+0 T:0x8ba0006c S:0x8ba03f1c] OM - Memory_alloc> return (0x8fa00458)
    [DSP] @0,071,593tk: [+0 T:0x8ba0006c S:0x8ba03f1c] OM - Memory_alloc> Enter(size=0xe)
    [DSP] @0,071,639tk: [+0 T:0x8ba0006c S:0x8ba03f1c] OM - Memory_alloc> return (0x8fa00470)
    [DSP] @0,071,694tk: [+0 T:0x8ba0006c S:0x8ba03ee4] OM - Memory_alloc> Enter(size=0x20)
    [DSP] @0,071,740tk: [+0 T:0x8ba0006c S:0x8ba03ee4] OM - Memory_alloc> return (0x8fa00480)
    [DSP] @0,071,791tk: [+0 T:0x8ba0006c S:0x8ba03eb4] OM - Memory_alloc> Enter(size=0x24)
    [DSP] @0,071,837tk: [+0 T:0x8ba0006c S:0x8ba03eb4] OM - Memory_alloc> return (0x8fa004a0)
    [DSP] @0,071,912tk: [+0 T:0x8ba0006c S:0x8ba03ecc] ti.sdo.ce.video1.VIDENC1 - VIDENC1_create> Enter (engine=0x0, name='h264fhdvenc', params=0x8fe038c0)
    [DSP] @0,071,993tk: [+0 T:0x8ba0006c S:0x8ba03e94] CV - VISA_create(0x0, 'h264fhdvenc', 0x8fe038c0, 0x2496, 'ti.sdo.ce.video1.IVIDENC1')
    [DSP] @0,072,066tk: [+0 T:0x8ba0006c S:0x8ba03d84] CV - VISA_create2(0x0, 'h264fhdvenc', 0x8fe038c0, 0x3c, 0x2496, 'ti.sdo.ce.video1.IVIDENC1')
    [DSP] @0,072,148tk: [+0 T:0x8ba0006c S:0x8ba03d1c] CE - Engine_open> Enter('local', 0x8ba03d6c, 0x8fe038c0)
    [DSP] @0,072,209tk: [+0 T:0x8ba0006c S:0x8ba03cfc] OM - Memory_alloc> Enter(size=0x2c)
    [DSP] @0,072,255tk: [+0 T:0x8ba0006c S:0x8ba03cfc] OM - Memory_alloc> return (0x8fa00510)
    [DSP] @0,072,310tk: [+0 T:0x8ba0006c S:0x8ba03d1c] CE - Engine_open> return(-1885338352)
    [DSP] @0,072,372tk: [+0 T:0x8ba0006c S:0x8ba03d64] OM - Memory_alloc> Enter(size=0x30)
    [DSP] @0,072,429tk: [+0 T:0x8ba0006c S:0x8ba03d64] OM - Memory_alloc> return (0x8fa00540)
    [DSP] @0,072,480tk: [+0 T:0x8ba0006c S:0x8ba03d3c] ti.sdo.ce.alg.Algorithm - Algorithm_create> Enter(fxns=0x8fac8194, idma3Fxns=0x0, iresFxns=0x8fac80ec, params=0x8fe038c0, attrs=0x8ba03e80)
    [DSP] @0,072,576tk: [+0 T:0x8ba0006c S:0x8ba03d1c] OM - Memory_alloc> Enter(size=0x10)
    [DSP] @0,072,623tk: [+0 T:0x8ba0006c S:0x8ba03d1c] OM - Memory_alloc> return (0x8fa00570)
    [DSP] @0,072,687tk: [+0 T:0x8ba0006c S:0x8ba03cfc] ti.sdo.fc.dskt2 - _DSKT2_init> Enter
    [DSP] @0,072,757tk: [+0 T:0x8ba0006c S:0x8ba03cfc] ti.sdo.fc.dskt2 - _DSKT2_init> Exit
    [DSP] @0,072,802tk: [+0 T:0x8ba0006c S:0x8ba03d0c] ti.sdo.fc.dskt2 - DSKT2_createAlg> Enter (scratchId=0, fxns=0x8fac8194, parentAlg=0x0, params=0x8fe038c0)
    [DSP] @0,072,880tk: [+0 T:0x8ba0006c S:0x8ba03c94] ti.sdo.fc.dskt2 - _DSKT2_init> Enter
    [DSP] @0,072,924tk: [+0 T:0x8ba0006c S:0x8ba03c94] ti.sdo.fc.dskt2 - _DSKT2_init> Exit
    [DSP] @0,072,969tk: [+0 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Enter (scratchId=0, fxns=0x8fac8194, parentAlg=0x0, params=0x8fe038c0, extHeapId=-1881130816, singleHeap=0)
    [DSP] @0,073,065tk: [+2 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> DSKT2_AlgAttrs extHeapId -1 and singleHeap 0
    [DSP] @0,073,135tk: [+2 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Num memory recs requested 12
    [DSP] @0,073,195tk: [+2 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> memTab allocated at 0x8fa00910 size=0xf0
    [DSP] @0,073,264tk: [+2 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Num memory recs requested 12
    [DSP] @0,073,325tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[0]: size=0x1ed8, align=0x1, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,073,405tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[1]: size=0x5c00, align=0x8, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,073,484tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[2]: size=0xc00, align=0x1, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,073,563tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[3]: size=0x5c00, align=0x1, space=IALG_EXTERNAL, attrs=IALG_SCRATCH
    [DSP] @0,073,642tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[4]: size=0x1400, align=0x1, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,073,722tk: [+4 T:0x8ba0006c S:0x8ba03c@3,626,603us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,626,829us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> return (0)
    @3,627,023us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7a3c, timeout=-1)
    @3,627,392us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
    a4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[5]: size=0x451c88, align=0x8, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,073,802tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[6]: size=0xc00, align=0x8, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,073,880tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[7]: size=0x6400, align=0x80, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,073,960tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[8]: size=0x99c, align=0x20, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,074,039tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[9]: size=0x100, align=0x20, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,074,117tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[10]: size=0x14, align=0x20, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,074,197tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Requested memTab[11]: size=0x8, align=0x20, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,074,277tk: [+0 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> Enter (scratchId=0, numRecs=12, extHeapId=0)
    [DSP] @0,074,346tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_usesInternalScratch> Enter (numRecs=12)
    [DSP] @0,074,404tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_usesInternalScratch> Exit (returnVal=1)
    [DSP] @0,074,460tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> Alg requires some Internal Scratch in group 0
    [DSP] @0,074,525tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> Allocate as much as possible in the memory space requested
    [DSP] @0,074,597tk: [+0 T:0x8ba0006c S:0x8ba03bd4] ti.sdo.fc.dskt2 - _DSKT2_initializeAndUseSharedScratch> Enter (scratchGroupId=0, numRecs=12)
    [DSP] @0,074,672tk: [+0 T:0x8ba0006c S:0x8ba03b84] ti.sdo.fc.dskt2 - _DSKT2_getScratchRequestInfo> Enter (ialgSpace=IALG_DARAM0, numRecs=12)
    [DSP] @0,074,754tk: [+0 T:0x8ba0006c S:0x8ba03b84] ti.sdo.fc.dskt2 - _DSKT2_getScratchRequestInfo> Exit (sizeBestCase=52488, sizeWorstCase=52696, numScratchRecs=5)
    [DSP] @0,074,879tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,074,943tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,074,998tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,075,061tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,075,115tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,075,178tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,075,232tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,075,295tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,075,349tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,075,412tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,075,471tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,075,535tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,075,588tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,075,651tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,075,705tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,075,768tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit@3,633,502us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,633,722us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> return (0)
    @3,633,909us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7a3c, timeout=-1)
    @3,634,218us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
     (status=TRUE)
    [DSP] @0,075,822tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,075,885tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,075,939tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Enter (scrBuffDesc->base=0x11818000)
    [DSP] @0,076,002tk: [+0 T:0x8ba0006c S:0x8ba03bb4] ti.sdo.fc.dskt2 - _DSKT2_useSharedScratch> Exit (status=TRUE)
    [DSP] @0,076,061tk: [+0 T:0x8ba0006c S:0x8ba03bd4] ti.sdo.fc.dskt2 - _DSKT2_initializeAndUseSharedScratch> Exit
    [DSP] @0,076,121tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Enter (index=0, ialgSpace=IALG_EXTERNAL, extHeapId=0)
    [DSP] @0,076,254tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Exit (returnVal=1)
    [DSP] @0,076,312tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[0] allocated in persistent memory in Memory space:IALG_EXTERNAL. Addr=0x8ba049e8
    [DSP] @0,076,399tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratchAddr> Enter (scratchMutexId=0, addr=0x11818000)
    [DSP] @0,076,469tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratch> Exit (status=1 )
    [DSP] @0,076,524tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[1] already allocated from Internal Scratch. Addr=0x11818000, Attrs=IALG_SCRATCH
    [DSP] @0,076,609tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Enter (index=2, ialgSpace=IALG_EXTERNAL, extHeapId=0)
    [DSP] @0,076,705tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Exit (returnVal=1)
    [DSP] @0,076,763tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[2] allocated in persistent memory in Memory space:IALG_EXTERNAL. Addr=0x8ba068c0
    [DSP] @0,076,849tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Enter (index=3, ialgSpace=IALG_EXTERNAL, extHeapId=0)
    [DSP] @0,077,110tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Exit (returnVal=1)
    [DSP] @0,077,168tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[3] allocated in persistent memory in Memory space:IALG_EXTERNAL. Addr=0x8ba074c0
    [DSP] @0,077,253tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Enter (index=4, ialgSpace=IALG_EXTERNAL, extHeapId=0)
    [DSP] @0,077,370tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Exit (returnVal=1)
    [DSP] @0,077,427tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[4] allocated in persistent memory in Memory space:IALG_EXTERNAL. Addr=0x8ba0d0c0
    [DSP] @0,077,513tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Enter (index=5, ialgSpace=IALG_EXTERNAL, extHeapId=0)
    [DSP] @0,126,905tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Exit (returnVal=1)
    [DSP] @0,126,972tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[5] allocated in persistent memory in Memory space:IALG_EXTERNAL. Addr=0x8ba0e4c0
    [DSP] @0,127,062tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratchAddr> Enter (scratchMutexId=0, addr=0x1181dc00)
    [DSP] @0,127,138tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratch> Exit (status=1 )
    [DSP] @0,127,196tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[6] already allocated from Internal Scratch. Addr=0x1181dc00, Attrs=IALG_SCRATCH
    [DSP] @0,127,281tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratchAddr> Enter (scratchMutexId=0, addr=0x1181e800)
    [DSP] @0,127,348tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratch> Exit (status=1 )
    [DSP] @0,127,402tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[7] already allocated from Internal Scratch.@3,640,403us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,640,627us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> return (0)
    @3,640,817us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7a3c, timeout=-1)
    @3,641,120us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
     Addr=0x1181e800, Attrs=IALG_SCRATCH
    [DSP] @0,127,487tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Enter (index=8, ialgSpace=IALG_EXTERNAL, extHeapId=0)
    [DSP] @0,127,594tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Exit (returnVal=1)
    [DSP] @0,127,652tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[8] allocated in persistent memory in Memory space:IALG_EXTERNAL. Addr=0x8be60160
    [DSP] @0,127,737tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratchAddr> Enter (scratchMutexId=0, addr=0x11824c00)
    [DSP] @0,127,805tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratch> Exit (status=1 )
    [DSP] @0,127,859tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[9] already allocated from Internal Scratch. Addr=0x11824c00, Attrs=IALG_SCRATCH
    [DSP] @0,127,944tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Enter (index=10, ialgSpace=IALG_EXTERNAL, extHeapId=0)
    [DSP] @0,128,019tk: [+0 T:0x8ba0006c S:0x8ba03c24] ti.sdo.fc.dskt2 - _DSKT2_allocateInDesignatedSpace> Exit (returnVal=1)
    [DSP] @0,128,076tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[10] allocated in persistent memory in Memory space:IALG_EXTERNAL. Addr=0x8be60b00
    [DSP] @0,128,178tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratchAddr> Enter (scratchMutexId=0, addr=0x11824d00)
    [DSP] @0,128,245tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_isSharedScratch> Exit (status=1 )
    [DSP] @0,128,300tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> memTab[11] already allocated from Internal Scratch. Addr=0x11824d00, Attrs=IALG_SCRATCH
    [DSP] @0,128,386tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_usesInternalScratch> Enter (numRecs=12)
    [DSP] @0,128,443tk: [+0 T:0x8ba0006c S:0x8ba03c44] ti.sdo.fc.dskt2 - _DSKT2_usesInternalScratch> Exit (returnVal=1)
    [DSP] @0,128,500tk: [+2 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> Increment scratch group 0`s reference count
    [DSP] @0,128,567tk: [+0 T:0x8ba0006c S:0x8ba03c4c] ti.sdo.fc.dskt2 - _DSKT2_incrScratchReferenceCount> Enter (scratchMutexId=0)
    [DSP] @0,128,636tk: [+0 T:0x8ba0006c S:0x8ba03c4c] ti.sdo.fc.dskt2 - _DSKT2_incrScratchReferenceCount> Exit
    [DSP] @0,128,690tk: [+0 T:0x8ba0006c S:0x8ba03c64] ti.sdo.fc.dskt2 - _DSKT2_assignInstanceMemory> Exit (returnVal=1)
    [DSP] @0,128,751tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[0]: base=0x8ba049e8, size=0x1ed8, align=0x1, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,128,840tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[1]: base=0x11818000, size=0x5c00, align=0x8, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,128,928tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[2]: base=0x8ba068c0, size=0xc00, align=0x1, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,129,016tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[3]: base=0x8ba074c0, size=0x5c00, align=0x1, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,129,105tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[4]: base=0x8ba0d0c0, size=0x1400, align=0x1, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,129,194tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[5]: base=0x8ba0e4c0, size=0x451c88, align=0x8, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,129,284tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[6]: base=0x1181dc00, size=0xc00, align=0x8, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,129,371tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[7]: base=0x1181e800, size=0x6400, align=0x80, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,129,460tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[8]: base=0x8be6016@3,647,001us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> Enter(queue=0x0, msg=0x442d8880)
    @3,647,216us: [+0 T:0x41bc8490 S:0x41bc79a4] OC - Comm_put> return (0)
    @3,647,404us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> Enter(queue=0x10000, msg=0x41bc7a3c, timeout=-1)
    @3,647,705us: [+0 T:0x41bc8490 S:0x41bc799c] OC - Comm_get> MSGQ_get() status=0x8000, return (0)
    0, size=0x99c, align=0x20, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,129,548tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[9]: base=0x11824c00, size=0x100, align=0x20, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,129,636tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[10]: base=0x8be60b00, size=0x14, align=0x20, space=IALG_EXTERNAL, attrs=IALG_PERSIST
    [DSP] @0,129,725tk: [+4 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> Allocated memTab[11]: base=0x11824d00, size=0x8, align=0x20, space=IALG_DARAM0, attrs=IALG_SCRATCH
    [DSP] @0,129,818tk: [+0 T:0x8ba0006c S:0x8ba03c6c] ti.sdo.fc.dskt2 - _DSKT2_enqueueMemTab> Enter (segId=1, memTabSize=240, numRecs=12, extHeapId=0)
    [DSP] @0,129,896tk: [+0 T:0x8ba0006c S:0x8ba03c6c] ti.sdo.fc.dskt2 - _DSKT2_enqueueMemTab> Exit (status=TRUE)
    [DSP] @0,135,188tk: [+7 T:0x8ba0006c S:0x8ba03ca4] ti.sdo.fc.dskt2 - DSKT2_createAlg3> algInit call failed -1
    [DSP] @0,135,244tk: [+0 T:0x8ba0006c S:0x8ba03c6c] ti.sdo.fc.dskt2 - DSKT2_freeAlg> Enter (scratchMutexId=0, alg=0x8ba049e8)
    [DSP] @0,135,308tk: [+2 T:0x8ba0006c S:0x8ba03c6c] ti.sdo.fc.dskt2 - DSKT2_freeAlg> Dequeue alg  information

  • I have found where the problem lies, h264fhdvenc's dataEndianMode is XDM_LE_32, but h264enc's is XDM_BYTE, SO shoud modify  params->dataEndianness = XDM_LE_32. in encoder demo!

  • Hi Zhangke,

    Did you make your "h264fhdenc" work?

    what is major issue?

    we have same problems, could you give us some suggestions.

    Thanks a lot!

    Yalei

     

  • Hi AC,

    Do you know how to solve this issues which is "h2.64fhdvenc" codec(1080P) cannot run correctly

    on DM6467?

    Thanks a lot!

    Yalei

  • HI

    I am encoding 1080p with h264fhdvenc codec.I have a problem with it .

     

    Error: Failed to encode video buffer

     

    Can you tell me how to deal it ?