Hi,
We have recently purchased EVMK2H.
The details about the board are as follows:
[00:00:43] BMC>ver
[00:00:43] Executing command "ver"
[00:00:43]
[00:00:43] BMC Version EVM Type EVM Superset EVM Subset EVM Version EVM S/N UCD Ver
[00:00:43] 1.0.2.6 0.0.0.1 K2KH-EVM XTCIEVMK2X 4.0 109467 A03
$ sudo python bmc_tool.py
[sudo] password for user:
104_A03
78_A03_02
52_A03_03
The board is working fine, however we have one doubt regarding the BMC "status" command.
When the board is up and running, after we issue a "status" command, subsequent "shutdown" and "run" commands seem to be failing.
More details: (BMC of the steps we took)
[00:00:00] BMC Init Begin
[00:00:00] BMC Version 1.0.2.6
[00:00:00] XTCIEVMK2X
[00:00:00] 4.0
[00:00:00] S/N: 109467
[00:00:00] BMC Init Complete
[00:00:00] Main PWR Start Begin
[00:00:00] Main PWR Start Complete
[00:00:00] SOC PWR Start Begin
[00:00:00] Testing register 0 of clock 1... Passed.
..... LOT OF DEBUG INFO
......
[00:00:02] Clock 3
[00:00:02] Passed
[00:00:02] SOC PWR Start Complete
[00:00:02] SOC RST Begin
[00:00:02] Current BootMode is set to DSP No-Boot
[00:00:02] SOC RST Complete
[00:00:02] BOOT COMPLETE
Now we issue "status" and followed by "shutdown"
[00:08:59] Executing command "status"
[00:08:59] Board State SOC State DIP SW SOC GPIO 6 & 7
[00:08:59] SOC State SOC Running 0001 00
[00:09:03] BMC>shutdown
[00:09:03] Executing command "shutdown"
[00:09:03] Full Reset Begin
[00:09:03] Full Reset Complete
[00:09:03] POR Begin
[00:09:03] POR Complete
[00:09:03] SOC PWR Stop Begin
[00:15:20] BMC>
No further messages come up. That is, "PWR Stop Complete" does not come up...
if we were to issue status again,
[00:15:22] BMC>status
[00:15:22] Executing command "status"
[00:15:22] Board State SOC State DIP SW SOC GPIO 6 & 7
[00:15:22] SOC State SOC Running 0001 00
following which we issue "shutdown" again and then BMC stops responding to any commands (other than just replying with the BMC> prompt)
[00:15:32] BMC>shutdown
[00:15:32] Executing command "shutdown"
[00:15:39] BMC>status
[00:15:42] BMC>status
BMC>
Could you kindly tell if this is to be expected?
Further, the hardware power push button also does not respond once a status command is issued.
Thanks and regards,