Hi,
Did anyone try WMA ENC on on OMAP3x DVSDK 3.01.00.10?
DVSDK 3.01.00.10 (could be the latest) supports WMA ENC/DEC?
There is no description in the release note to support WMA ENC/DEC feature, just AAC and MP3.
I think thar it's possible to do that but need to make sure WMA capability on DVSDK.
¨ Audio: AAC LC/HE Decoder, AAC LC/HE Encoder, MP3 Decoder
¨ Image: JPEG Encoder/Decoder
¨ Speech: G.711 Encoder/Decoder
¨ Video: H.264 BP Encoder/Decoder, MPEG4 SP Encoder/Decoder, MPEG2 Decoder
¨ De-interlacer - Converts the YUV422 interlaced frames to YUV422 progressive frames
Regards,
Kasuya