Other Parts Discussed in Thread: TMS320DM6467
Dear all,
My new TMS320DM6467 EVM got two strange problems:
1.
The output contain some messy code when I connect the board to a console window with Hyper terminal and power on the board. Also, the input is abnormal in the state of u-boot or linux shell of the board.
When I input some command and pressed enter, the result is unpredictable, it will print some part of the result(such as 'printenv' in u-boot) which may lose some character(Please look up the accessories), or it will be unactived unless I press several times of enter.
The picture below was in the state of kernel shell.

The picture below was in the state of u-boot
2.
I've install the hardware according to the Getting Started Guide(Such as HD input video source, HD output display and SW3, etc), but the Standalone mode have no representation, the Standalone demo can not run successfull. I make sure that my display equipment and hardware setting up are correct.
What can I do in the next step?
Look for your generous help! Thank you!
Best Wishes
Shaofei