Other Parts Discussed in Thread: OMAP-L137
Hi,
Is it necessary to use a buffer between the Ehternet PHY and OMAP-L13x ?
According to the OMAP-L137 EVM's schematic here, the PHY KSZ8893MQL is connected to OMAP through
a Bus Exchange switch(SN74CBTLV16212DGGR).
According to the datasheet of KSZ8893(Page 103),
with regards to PHYs SNI Transmit to OMAP the Ouput Valid minimum time is "0ns"
On the other hand regarding the OMAP's (MDIO_CLKH-MDIO)- Hold time,
the datasheet(Page 108-109) of OMAP-L13x mentions that, MDIO_D data input valid after MDIO_CLK high min i.e th(MDIO_CLKH-MDIO) = 10 ns.
Please let me know whether we should have a 10ns buffer between the PHY and OMAP (EVM doesn't implement such delay logic).
Thankyou in advance
Regards.