Part Number: TMS320C6657
Hello,
I am trying to interface an FPGA Kintex7 Ultrscale to the DSP through the EMIF-16 interface looking at the Standard EMIF documentation I can see that the timing relationship of the EMIF outputs with the AECLKOUT from the DSP to the external interface is defined in the document (spruek6b.pdf ) but no such timing relationship is given for the EMIF-16 signals (sprugz3a.pdf). Should I consider the same timing information of the EMIF-16 signals as the standard EMIF ones with respect to the AECLKOUT.
Regards,
Fatima