This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3358: Ethernet/IP on Linux

Part Number: AM3358
Other Parts Discussed in Thread: SYSBIOS

Tool/software: Linux

Team, can you please help answer question for my customer:

 

1. Ideally we would like to run Linux.  Out of the box we plan on using QT to run the touchscreen display and down the road we are looking to add a web server.  So access to the open source world is important.

a.      Can we use the PRU-ICSS components to handle EtherNET/IP while having the main ARM processor run Linux?  Or do we have to use SYSBIOS to make use of the PRU-ICSS?

2.      If the answer to question 1.a is we have to run SYSBIOS…

a.      Can we run QT 5.7 OPENGL on SYSBIOS?

 

Thanks

Viktorija