This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms320dm647 Local Reset hangs



We are booting dm647 from a host over pci. We use the Local Reset to initialize the dsp before loading code and de-asserting the Local Reset. Occasionally when performing the Local Reset in preparation for re-loading a dsp with an application, our code times out waiting for the LRSTDONE!

Here's the host's routine to perform the Local Reset. The dm647_read/writereg routines are accessing the dsp registers over pci.

static void dm647_local_reset(dm647_t *dsp)
{
    u32 reg;
    int timeout = 1000;

    reg = dm647_readreg(dsp, DM647_PSC_MDSTAT33_ADR);
    /* assert local reset bit */
    dm647_writereg(dsp, DM647_PSC_MDCTL33_ADR, reg & ~DM647_PSC_MDCTL33_LRST);
    au_sync();    /* cpu pipeline flush */
    /* spin, waiting for reset to be indicated */
    while (--timeout) {
        msleep(1);
        if ((dm647_readreg(dsp, DM647_PSC_MDSTAT33_ADR) & DM647_PSC_MDSTAT33_LRSTDONE))
            break;
    }

    if (timeout==0)
        DM647_SERR(dsp, "%s: Timed out waiting for local reset", __func__);
}

Are we missing something? Do we need to perform some additional action to reset the dsp before loading new code?

Thanks, Geoff