Part Number: AM3359
Other Parts Discussed in Thread: AM3359
Tool/software: Starterware
Hi,
I am using AM3359 Industrial Communications Engine development board. As beginning, I tried to write simple code to demo using it.
The simple hello code project I created it from blank, and it can run on debug mode normally.
When I added LED ON/OFF sample code (which from AM335X_StarterWare_02_00_01_01) to it, and then the code ran into other location when it ran into those sample function. It looks my project does not have the right .cmd file. The current .cmd file is from project setup generated automatically.
In the starterware package, I saw some command file, but from the header comment they are for TMS470, not for AM335X.
Would anyone have AM3359 Industrial Communications Engine specific command file?
Best,
Gansheng